Other Parts Discussed in Thread: UNIFLASH, MOTORWARE
dear, plesae I need to know:
1- how can I re-flash the f28035 to run with the gui after i worked with sensorless ACI? or i donot need to this step?
i didnot under stand the folllowing:
install J9, power board, connect USB JTAG, launch CCSv4
-----
delete all other projects (right click, delete)
---
view -> targets -> user defined
make sure xds100-f28035[default]
make sure no targets under projects folder
---
launch debug (green bug)
connect target
target -> load program 2xPM_Motors.out
where is found the program 2xPM_Motors.out
2- i need to know what are jumbers which i need for work with the F28069 controller: i need hw configration because i did not undrerstand
what is the mode of gui?
3- i need with GUI to plot the rotor flux, how can I plot it? F2806xISO GUI?