Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I wished to test out C2000, and thought to buy the USB Controlstick,
I wanted to know more about it, as I needed to use Quadrature Encoder Pins, and Motor Control features which is why I decided on c2000 (I heard motor control libraries are supposed to be good). So, I installed controlSUITE, to find out more (as was written on the website). I couldn't find much info other than examples and some features.
It never mentioned whether UART, i2c, and CAN communication can be done using those 32 pins on the stick. nor does it mention about the Quadrature pins ... do I assume it doesn't have the features ? (even though the ICs data sheet says it has?)
Anyone have any idea whether it has these features ?