What register/value tells the ePWM to be active high? I am happy to "read the funny manual" if I can get pointed to the right manual.
According to the SPRUH18D (page 273) it appears that setting this 2 bit field (EPwm1Regs.AQCTLA.bit.CAU) to “AQ_CLEAR” makes the ePWM to be active high. It also sets EPwm1Regs.AQCTLA.bit.ZRO to "AQ_SET". Are both required in order to get the ePWM module to be active high.
Page 276 EPwm1Regs.AQCTLA.bit.PRD is set to AQ_CLEAR as part of setting the ePWM module to be active low. What should it be to get active high?
In one of the example projects it sets the CAU to CLEAR and CAD to SET. What is the role of CAD?