Other Parts Discussed in Thread: CCSTUDIO
I'm currently trying to use the HVMotorCtrl+PfcKit_v1.7 with C2000 Microcontroller but instead I want to use GUI Composer to alter how the motor operates compared to the default GUI. I went to HVPM_Sensored folder to build the GUI since the c++ file is located there to control the Permanent Synchronous Motor. I'm trying to get it to function with the speedRef variable in a dial GUI but I got a connection error when used in conjunction with HVMTRPFCKIT-GUI-FlashImagev1.out when flashed:
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.
I was wondering if anyone knows what I'm doing wrong or what I need to do to fix this issue.