Other Parts Discussed in Thread: CONTROLSUITE
I finaly got my c28 project to build without errors now working on M3.
In the M3 project, I have several persistent errors and warnings. two errors and two warnings are in the file F28M35x_Adc.c
two are on comments lines: 29, 30 see below
// CPU_RATE define statement in the F28M35xA_Examples.h file must
// contain the correct CPU clock period in nanoseconds.
the error is the same for both lines
Multiple markers at this line
- explicit type is missing ("int"
assumed)
I also get the very same errors and warnings for the following two lines 29, 30 in the file F28M35x_Device.h
extern cregister volatile unsigned int IFR;
extern cregister volatile unsigned int IER;
I get a fifth warning in file LVMA_M3.c on line 796
IntRAMRegister(FAULT_SYSTICK,SysTickIntHandler);
function declared implicitly
and a sixth warning in file httpd.c line77
static int command;
function declared implicitly
I am sure the IntRAMRegister warning is behind the errors, but can't locate in what file the function exists. Any guidance would be much appreciated.