Other Parts Discussed in Thread: MOTORWARE, DRV8301, DRV8312, CONTROLSUITE, SYSBIOS
Hi
I am using MotorWare 1.1.0.6 with DRV8301-HC-EVM-RevD and the F2806x ControlCard.
I launched the GUI, setup the identify motor parameters for my motor.
I am running in speed mode.
When I start the motor and play with different speeds it all works fine, smooth operation.
When I load the motor shaft I see the torque and current increase accordingly, and when the load is removed the motor goes back to normal operation.
The problem I have is as follows:
I command a speed of 0 rpm (under no load the shaft doesn't move and there is some resistance if I try to turn it)
I can turn the shaft by hand past a point where the motor controller becomes unstable and no longer maintains 0 rpm when I release the shaft.
It sometimes turns backwards, sometimes forwards, and more concerning sometimes vibrates and jerks through different shaft positions.
This is an 8 pole (4 pole pairs) , 30A motor with a 3200 Max RPM (motor max freq set at 250).
Kp is automatically set at 3.75 and Ki set at 0.0375 (speed loop tuning)
Please let me know if there's something I am missing here.
Thanks
Dhar