Other Parts Discussed in Thread: TMS320F28335
Hi all,
Don't exist port of comunication RS232 in TMS320f28335 implemented as hardware and I need this port.
Can you use any software library to communicate by RS232?
Thanks and regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F28335
Hi all,
Don't exist port of comunication RS232 in TMS320f28335 implemented as hardware and I need this port.
Can you use any software library to communicate by RS232?
Thanks and regards.
Hi!
You can use SCI (UART).
// TI File $Revision: /main/3 $
// Checkin $Date: April 21, 2008 16:04:59 $
//###########################################################################
//
// FILE: Example_2823xSci_FFDLB_int.c
//
// TITLE: DSP2823x Device SCI Digital Loop Back porgram.
//
//
// ASSUMPTIONS:
//
// This program requires the DSP2823x header files.
//
// This program uses the internal loop back test mode of the peripheral.
// Other then boot mode pin configuration, no other hardware configuration
// is required.
//
// As supplied, this project is configured for "boot to SARAM"
// operation. The 2823x Boot Mode table is shown below.
// For information on configuring the boot mode of an eZdsp,
// please refer to the documentation included with the eZdsp,
//
// $Boot_Table:
//
// GPIO87 GPIO86 GPIO85 GPIO84
// XA15 XA14 XA13 XA12
// PU PU PU PU
// ==========================================
// 1 1 1 1 Jump to Flash
// 1 1 1 0 SCI-A boot
// 1 1 0 1 SPI-A boot
// 1 1 0 0 I2C-A boot
// 1 0 1 1 eCAN-A boot
// 1 0 1 0 McBSP-A boot
// 1 0 0 1 Jump to XINTF x16
// 1 0 0 0 Jump to XINTF x32
// 0 1 1 1 Jump to OTP
// 0 1 1 0 Parallel GPIO I/O boot
// 0 1 0 1 Parallel XINTF boot
// 0 1 0 0 Jump to SARAM <- "boot to SARAM"
// 0 0 1 1 Branch to check boot mode
// 0 0 1 0 Boot to flash, bypass ADC cal
// 0 0 0 1 Boot to SARAM, bypass ADC cal
// 0 0 0 0 Boot to SCI-A, bypass ADC cal
// Boot_Table_End$
//
// DESCRIPTION:
//
// This program is a SCI example that uses the internal loopback of
// the peripheral. Both interrupts and the SCI FIFOs are used.
//
// A stream of data is sent and then compared to the recieved stream.
//
// The SCI-A sent data looks like this:
// 00 01 02 03 04 05 06 07
// 01 02 03 04 05 06 07 08
// 02 03 04 05 06 07 08 09
// ....
// FE FF 00 01 02 03 04 05
// FF 00 01 02 03 04 05 06
// etc..
//
//
// The SCI-B sent data looks like this:
// FF FE FD FC FB FA F9 F8
// FE FD FC FB FA F9 F8 F7
// FD FC FB FA F9 F8 F7 F6
// ....
// 01 00 FF FE FD FC FB FA
// 00 FF FE FD FC FB FA F9
// etc..
//
// Both patterns are repeated forever.
//
// Watch Variables:
//
// SCI-A SCI-B
// ----------------------
// sdataA sdataB Data being sent
// rdataA rdataB Data received
// rdata_pointA rdata_pointB Keep track of where we are in the datastream
// This is used to check the incoming data
//###########################################################################
// Original Source by S.D.
//
// $TI Release: DSP2833x/DSP2823x Header Files V1.20 $
// $Release Date: August 1, 2008 $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
//#define SCIA_INTERNAL_LOOPBACK
#define CPU_FREQ 150E6
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 100E3
#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.
interrupt void sciaTxFifoIsr(void);
interrupt void sciaRxFifoIsr(void);
interrupt void scibTxFifoIsr(void);
interrupt void scibRxFifoIsr(void);
void scia_fifo_init(void);
void scib_fifo_init(void);
void error(void);
// Global variables
Uint16 sdataA[8]; // Send data for SCI-A
Uint16 sdataB[8]; // Send data for SCI-B
Uint16 rdataA[8]; // Received data for SCI-A
Uint16 rdataB[8]; // Received data for SCI-A
Uint16 rdata_pointA; // Used for checking the received data
Uint16 rdata_pointB;
#ifndef SCIA_INTERNAL_LOOPBACK
Uint16 sdata_pointA;
#endif // #ifndef SCIA_INTERNAL_LOOPBACK
void main(void)
{
#ifdef SCIA_INTERNAL_LOOPBACK
Uint16 i;
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();
// Setup only the GP I/O only for SCI-A and SCI-B functionality
// This function is found in DSP2833x_Sci.c
InitSciGpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
PieVectTable.SCITXINTA = &sciaTxFifoIsr;
PieVectTable.SCIRXINTB = &scibRxFifoIsr;
PieVectTable.SCITXINTB = &scibTxFifoIsr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
scia_fifo_init(); // Init SCI-A
#ifdef SCIA_INTERNAL_LOOPBACK
scib_fifo_init(); // Init SCI-B
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
// Step 5. User specific code, enable interrupts:
#ifdef SCIA_INTERNAL_LOOPBACK
// Init send data. After each transmission this data
// will be updated for the next transmission
for(i = 0; i<8; i++)
{
sdataA[i] = i;
}
for(i = 0; i<8; i++)
{
sdataB[i] = 0xFF - i;
}
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
#ifdef SCIA_INTERNAL_LOOPBACK
rdata_pointA = sdataA[0];
rdata_pointB = sdataB[0];
#else // #ifdef SCIA_INTERNAL_LOOPBACK
rdata_pointA = 0;
sdata_pointA = 0;
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
// Enable interrupts required for this example
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx1=1; // PIE Group 9, int1
PieCtrlRegs.PIEIER9.bit.INTx2=1; // PIE Group 9, INT2
PieCtrlRegs.PIEIER9.bit.INTx3=1; // PIE Group 9, INT3
PieCtrlRegs.PIEIER9.bit.INTx4=1; // PIE Group 9, INT4
IER = 0x100; // Enable CPU INT
#ifndef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCIFFTX.bit.TXFFIENA = 0; // disable TX interrupt
#endif // #ifndef SCIA_INTERNAL_LOOPBACK
EINT;
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;);
}
void error(void)
{
asm(" ESTOP0"); // Test failed!! Stop!
for (;;);
}
interrupt void sciaTxFifoIsr(void)
{
#ifdef SCIA_INTERNAL_LOOPBACK
Uint16 i;
for(i=0; i< 8; i++)
{
SciaRegs.SCITXBUF=sdataA[i]; // Send data
}
for(i=0; i< 8; i++) //Increment send data for next cycle
{
sdataA[i] = (sdataA[i]+1) & 0x00FF;
}
#else // #ifdef SCIA_INTERNAL_LOOPBACK
while (sdata_pointA != rdata_pointA)
{
if (SciaRegs.SCIFFTX.bit.TXFFST == 16)
{
break;
}
SciaRegs.SCITXBUF = rdataA[sdata_pointA]; // Send data
sdata_pointA++;
if (sdata_pointA >= sizeof(rdataA))
{
sdata_pointA = 0;
}
}
SciaRegs.SCIFFTX.bit.TXFFIENA = 0; // disable TX interrupt
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear SCI Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}
interrupt void sciaRxFifoIsr(void)
{
#ifdef SCIA_INTERNAL_LOOPBACK
Uint16 i;
for(i=0;i<8;i++)
{
rdataA[i]=SciaRegs.SCIRXBUF.all; // Read data
}
for(i=0;i<8;i++) // Check received data
{
if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) ) error();
}
rdata_pointA = (rdata_pointA+1) & 0x00FF;
#else // #ifdef SCIA_INTERNAL_LOOPBACK
rdataA[rdata_pointA] = SciaRegs.SCIRXBUF.all; // Read data
rdata_pointA++;
if (rdata_pointA >= sizeof(rdataA))
{
rdata_pointA = 0;
}
SciaRegs.SCIFFTX.bit.TXFFIENA = 1; // enable TX interrupt
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
SciaRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
void scia_fifo_init()
{
SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCICTL2.bit.RXBKINTENA =1;
#if 0
SciaRegs.SCIHBAUD = 0x0000;
SciaRegs.SCILBAUD = SCI_PRD;
#else
{
long temp;
// setup baud rate
// formula = lspclk/(baud*8) - 1;
temp = 25000000L / (115200 * 8) - 1;
SciaRegs.SCIHBAUD = (temp>>8) & 0xFF;
SciaRegs.SCILBAUD = (temp) & 0xFF;
}
#endif
#ifdef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
#else // #ifdef SCIA_INTERNAL_LOOPBACK
ScibRegs.SCIFFTX.bit.TXFFIENA = 0; // disable TX interrupt
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
#ifdef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCIFFTX.all=0xC028;
SciaRegs.SCIFFRX.all=0x0028;
#else // #ifdef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCIFFTX.all=0xC02e;
SciaRegs.SCIFFRX.all=0x0021;
#endif // #ifdef SCIA_INTERNAL_LOOPBACK
SciaRegs.SCIFFCT.all=0x00;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;
SciaRegs.SCIFFRX.bit.RXFIFORESET=1;
}
interrupt void scibTxFifoIsr(void)
{
Uint16 i;
for(i=0; i< 8; i++)
{
ScibRegs.SCITXBUF=sdataB[i]; // Send data
}
for(i=0; i< 8; i++) //Increment send data for next cycle
{
sdataB[i] = (sdataB[i]-1) & 0x00FF;
}
ScibRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}
interrupt void scibRxFifoIsr(void)
{
Uint16 i;
for(i=0;i<8;i++)
{
rdataB[i]=ScibRegs.SCIRXBUF.all; // Read data
}
for(i=0;i<8;i++) // Check received data
{
if(rdataB[i] != ( (rdata_pointB-i) & 0x00FF) ) error();
}
rdata_pointB = (rdata_pointB-1) & 0x00FF;
ScibRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
void scib_fifo_init()
{
ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.bit.TXINTENA =1;
ScibRegs.SCICTL2.bit.RXBKINTENA =1;
#if 0
SciaRegs.SCIHBAUD = 0x0000;
SciaRegs.SCILBAUD = SCI_PRD;
#else
{
long temp;
// setup baud rate
// formula = lspclk/(baud*8) - 1;
temp = 25000000L / (115200 * 8) - 1;
SciaRegs.SCIHBAUD = (temp>>8) & 0xFF;
SciaRegs.SCILBAUD = (temp) & 0xFF;
}
#endif
ScibRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
ScibRegs.SCIFFTX.all=0xC028;
ScibRegs.SCIFFRX.all=0x0028;
ScibRegs.SCIFFCT.all=0x00;
ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
ScibRegs.SCIFFTX.bit.TXFIFOXRESET=1;
ScibRegs.SCIFFRX.bit.RXFIFORESET=1;
}
//===========================================================================
// No more.
//===========================================================================
Regards,
Igor
Thank you very much Igor,
But I have o problem, I use the TMDSHVMTRPFCKIT and the SCI port is used for the USB comunication.
I need some library that understands the RS232 protocol and be able to communicate via the GPIO. In
micropic exist this type of library for pics and don't need specific hardware.
Regards.
Hi
Yes, I know, but the GPIO 19 and GPIO 18 is used for (SPI), and the rest of GPIO
for SCI is used for PWM. The GPIO 62 and GPIO 63 is not used but it's impossible connect to the kit.
So I need the library, if exist.
Thanks.
Hi!
And how about GPIO14,15 or 22,23 for SCI-B? Is it impossible to connect too?
Igor
There are numerous UART implementations on the net. Ex: http://supp.iar.com/Support/?note=88469
Generally search for "software UART"
Please remember that RS-232 defines not only logical serial interface but electrical standard as well.
Regards,
Maciej