Hi,
I am having issues in programming a F28335 on a custom board on Flash with CCS 3.3 (I know it's an old version of code composer but all of our testing settings and interfaces in the lab use it). We are using a xds510USB emulator from Spectrum. The program works fine with emulator connected, but once I disconnect it and power up the board the program does not start, all the pins have been checked and the 4 gpio for the boot are all pulled up. We tried then to use the flashing leds example using ccs5 and it works fine also when the emulator is disconnected and the board is powered up again. I think I am missing some files or options in the ccs 3.3 version.
Thanks in andvance.