Other Parts Discussed in Thread: DRV8301, MOTORWARE, DRV8312
Hi,
I just started with setting up the Insta Spin Motion development kit together with the GUI Composer v1. I use the following boards:
- drv8301kit_revD
- TMS320F28069MPZT
When I start the GUI composer the program is loaded properly on the controller and the console outputs ends with 'Restart Completed' (As it should be). However the hardware is not identified as you can see in the figure below. Furthermore the Leds 2 and 3 on the controller board (TMS320F28069MPZT) are red.
Question 1: How can I ensure that the hardware is properly identiefied?
Question 2: Where can I find the meaning of the status leds and how can I fix that?
(I assume that Questions 1 and 2 belong to the same problem.)
Kind regards,
Timon