I have been able to get the example flash_prog example to work, but cannot get the assembler to insert the F021_API_CortexM3_LE.lib into ram. My cmd file segment is:
/* Section allocation in memory */
SECTIONS
{
.intvecs: > INTVECS
.resetisr: > RESETISR
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.dload : > FLASH_DLOAD
.vtable : > C0_1
.data : > C0_1
.bss : > C2_3
.sysmem : > C0_1
.stack : > C0_1
.z1secvalues : > CSM_ECSL_Z1
.z1_csm_rsvd : > CSM_RSVD_Z1
.z2secvalues : > CSM_ECSL_Z2
.z2_csm_rsvd : > CSM_RSVD_Z2
GROUP
{
ramfuncs
{
-l F021_API_CortexM3_LE.lib
}
} LOAD = FLASHLOAD,
RUN = C0_1,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0
GROUP : > MTOCRAM
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CTOMRAM
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}
The .lib file cannot be found. Also, a warning saying no matching section. I am using compiler version 4.9.7 , running on CCS4.2.5. I tested the flash_prog example also on CCS4.2.5 but with compiler 4.6.6 and it works. But my application otherwise is working with compiler 4.9.7, and will not migrate to 4.6.6 without errors. How do I modify the example to get it to work on the newer compiler?
Any help, please.
Thanks,
Pat