Other Parts Discussed in Thread: DRV8312, INSTASPIN-BLDC
I have the DRV8312 kit with both the C2000 and Stellaris controlCARDs. The C2000 controlCARD works fine but I'm not overly impressed with InstaSPIN-FOC. I'm now trying to run InstaSPIN-BLDC on the Stellaris controlCARD and its not working properly. I've removed all the other Texas Instruments software versions and followed the installation instructions for the DRV8312-LM4F-BLDC. The GUI runs up but 95% of the time it fails to connect to the device. When it does connect I am able to start the motor but it stops again a few seconds later with the GUI reporting some kind of timeout. However, if I unplug the USB connection once the motor is running it will continue running indefinitely.