Dear Chris,
now we will try the Kit, the DC Connection is PVDD and GND which one in plus and which one minus? I have installed GUI_Composer_instaspin on the PC. What should i do first connect the J1 to Pc? Or should i connect the card on the power supply for example 12V and 80 A on the powersupply? Or should i switch on the power supply later?
I have tried without power suppy just with connection over USB J1 to Pc and i have this problem:
If i start the InstaSpin.exe.......Console Output:
Restarting Program Model... Initializing target : C:\ti\guicomposer\webapps\InstaSPIN_FOC_F2806xM\appConfig.ccxml Connecting target: Texas Instruments XDS100v2 USB Emulator_0/C28xx sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.
What can i try? Maybe connect to the power suppy or should that work without extern power?
thanks for help