This is Raheem basha.s from ansula. I try to interface that 28035 control card with cc studio4.2.4 that target is not detected.
i able to find TRSTn,TCK,TMS,TDI,TDO,VCC,GND pins in that PLC experiment kit/development tool
(with remove 28069 control card and ANALOG ip chip just for USB JTAG connection in that kit)
i check that interface is ok with above pins in F28035 control board, and that kit JTAG pin configuration its fine.
i check power connection in F28035 board its 3.3v at all vcc points.led is glowing
but when i connected to laptop with USB cable to kit and kit JTAG to control card JTAG connections and open cc studio tool and try for gpio toggle program then i get below errors.
Thanks & Regards,
RAHEEM BASHA.S