Other Parts Discussed in Thread: TMS320F28035, CONTROLSUITE
I'm using CCS 5.3 with a XDS100 v1 docking station and a TMS320F28035 control card in the docking station.
I can connect to an open loop hardware setup with the XDS100 v1 docking station... but when I move the the lab and try to connect to a different XDS100 v1 that has been put into a closed loop hardware setup for PFC I can NOT connect to the TMS320F28035 control card in the docking station.
I want to know what GPIO or JTAG pins have to be high and which ones have to be low for debuging.
This is what I have for voltage readings on my JTAG header on the open loop docking station that works.
J2
|`````````````````|
| 0v 0v |
| 0v 3.3v |
| 0v 3.3v |
| 0v 3.0v |
| N/C 3.3v |
| 0v 3.3v |
| 3.0v 3.3v |
```````````````````
JTAG
This is what I have for voltage readings on my JTAG header on the closed loop docking station that does NOT connect.
J2
|`````````````````|
| 0v 0v |
| 0v 3.3v |
| 0v 3.3v |
| 0v 3.0v |
| N/C 3.3v |
| 0v 3.3v |
| 2.5v 3.3v |
```````````````````
JTAG
the difference is 3.0v on the open loop dock station and 2.5v on the closed loop dock station on pin 6 of J2.
I'm going to try and pull up the voltage level on that 2.5v pin and see if that allows me to connect, but if that doesn't work I don't know what to do.
This is the error: Error connecting to the target: (Error -151 @ 0x0)