Hello,
I would like to make a BLDC driver with F2806x MCU and DRV8301 driver. The BLDC driver has to be UL certified.
So I'm testing DRV8301-HC-EVM rev D kit with F28069M control card.
Regarding that, I have few questions
1) I would like to know if the source code provide by TI could be used for the UL certification ?
2) Are the labs of instaSPIN FOC a good starting point (good template) for my project ?
3) In these labs, i didn't find the DRV8301 SPI driver, where is it handle?
4) My BLDC driver has to operate in 4 quadrans, currently the swithcing power supply is going down during the deceleration phase. Do you have a better idea than a braking resistor?
Thank you in advance,