I am looking at sensor hub functional description and it says - 100% hardware compatible with C2000 Launchpad. But J1.6 on Sensor hub is an interrupt-able pin for light sensor and on c2000 Launchpad J1.6 is ADCINA4 (Just analog pin). Can an analog pin be operated as GPIO (e.g ADCIN4) if not then how to get 100% hardware compatibility between C2000 LP and sensor hub.
RBG