Hi,
I am using a buffer of size [1000] and single time plot property in CCS 5. I would like to know if it is possible to sync. the graph with the buffer such as the buffer is plotted after writing the last word to it before it wrap around. As you can see in the figure below there is a dip in the graph which is an old value in the buffer.
Thanks,
Nezar