I have a motor with 10 pole pairs and encoder with 500 lines (resolution 2000). Ther is a transmission between encoder and motor - when the motor has one revolution, the encoder has three. I tried to define USER_MOTOR_ENCODER_LINES 1500 (3 x 500) but no success. I think the problem is, that the software sees 3 pulses from index by 1 revolution.
Is it possible to mask 2 of the 3 pulses from index?
I use the motorware v1.01.00.07 - Lab 12 / F28069MISO controlCard + DRV8301 Drive
Uwe