This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program will not fit into available memory

Hello,

I'm developing a project using a TMS28335 microcontroller, but I'm new in these topics so I've just copied some code from several examples.

I'm running a program from FLASH memory, and I was defining an array of size 2048 without having problems, but now I need to change its size to 4200 but I got this error:

program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x1048 page 1. Available memory ranges: F28335_FLASH_FlashingLeds.CMD /Prueba3 line 146 C/C++ Problem

My code is:

Uint16 Aux1;
Uint16 Datos[TAM]; // where TAM is 2048 and I need it to be 4200
Uint32 Suma;
Uint32 Promedio;
Uint16 DatoRec;

I suppose that section .ebss has not enough space to include all the variables, so my question is, how could I change the section where variables are assigned?

This could be a simple question, but I'm really confused with all this programming, that's why I have copied some example code sections.

Thanks for your help.

  • Hello, Christian.

    If you use "Datos" as read-write array, it must be placed only in the memory (.ebss, by the compiler). Otherwise, please use "const" modifier to put "Datos" to the FLASH.

    For the available memory mappings, please refer to the sprs439m.pdf, page 35. You have 32k (in words, 16 bit) memory for use by program and data.

    Please, show your linker script (F28335_FLASH_FlashingLeds.CMD). To fit your data, you need to extend ".ebss" section in a way:

         .ebss : > RAML4 | RAML5   PAGE = 1

    instead of default one:

         .ebss : > RAML4  PAGE = 1

    Array of size 2048 is 0x800 words and will take just a half of the RAML4. When you grow your array to 4200 you'll take 0x1068 words of the maximum 0x1000 words available per memory block.

    Hope this helps.

  • Hello Christian!

    Try to make the following changes to the file F28335_FLASH_FlashingLeds.CMD:

    .ebss : > RAML45 PAGE = 1
    data : > RAML45 PAGE = 1

    ...................................................


    SECTIONS
    {
    Net_terminals: > RAML45,PAGE = 1
    Controller: > RAML45,PAGE = 1
    IBx_addr: > RAML45,PAGE = 1
    Buck1Loop: > RAML45,PAGE = 1
    Buck2Loop: > RAML45,PAGE = 1
    DataLogTST: > RAML45,PAGE = 1
    GraphData: > RAML45,PAGE = 1

    }

    Regards,

    Igor

  • Hello Anton and Igor,

    Thanks for your answers, I've changed my CMD file at the .ebss part.

    Trying with:

    .ebss : > RAML45   PAGE = 1 

    makes I still got the following error:

    no valid memory range(NULL) available for placement of ".ebss" F28335_FLASH_FlashingLeds.CMD /Prueba3 line 146 C/C++ Problem

    I'm using CCSv5, by the way. Changing the code to:

    .ebss : > RAML4 | RAML5   PAGE = 1

    now gives me this error:

    program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x10b0 page 1. Available memory ranges: RAML4 size: 0x1000 unused: 0x1000 max hole: 0x1000 RAML5 size: 0x1000 unused: 0x1000 max hole: 0x1000 F28335_FLASH_FlashingLeds.CMD /Prueba3 line 146 C/C++ Problem

    I also have 2 questions:

    1. If I change the line that starts with .ebss, I must change the line that starts with data, and all the lines at SECTIONS, as Igor suggested?

    2. Additional to the data I have, I need to declare more variables. Which memory section could I join to RAML4 and RAML5, when solved the actual problem?

    /*
    // TI File $Revision: /main/9 $
    // Checkin $Date: August 28, 2007   11:23:38 $
    //###########################################################################
    //
    // FILE:	F28335.cmd
    //
    // TITLE:	Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: DSP2833x Header Files V1.00 $
    // $Release Date: September 7, 2007 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file, 
    // add the header linker command file directly to the project. 
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within 
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //   
    // For BIOS applications add:      DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2833x_Headers_nonBIOS.cmd    
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the 
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper 
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
       library search path under project->build options, linker tab, 
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28335  
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
        Notes: 
              Memory blocks on F28335 are uniform (ie same
              physical memory) in both PAGE 0 and PAGE 1.  
              That is the same memory region should not be
              defined for both PAGE 0 and PAGE 1.
              Doing so will result in corruption of program 
              and/or data. 
              
              L0/L1/L2 and L3 memory blocks are mirrored - that is
              they can be accessed in high memory or low memory.
              For simplicity only one instance is used in this
              linker file. 
              
              Contiguous SARAM memory blocks can be combined 
              if required to create a larger memory block. 
     */
    
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
       RAML0       : origin = 0x008000, length = 0x001000     /* on-chip RAM block L0 */
       RAML1       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L1 */
       RAML2       : origin = 0x00A000, length = 0x001000     /* on-chip RAM block L2 */
       RAML3       : origin = 0x00B000, length = 0x001000     /* on-chip RAM block L3 */
       ZONE6       : origin = 0x0100000, length = 0x100000    /* XINTF zone 6 */ 
       ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 
       FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
       FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
       FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */
       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */
       FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
       FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
       FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
       OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
       ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
       
       IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
       FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML4       : origin = 0x00C000, length = 0x001000     /* on-chip RAM block L1 */
       RAML5       : origin = 0x00D000, length = 0x001000     /* on-chip RAM block L1 */
       RAML6       : origin = 0x00E000, length = 0x001000     /* on-chip RAM block L1 */
       RAML7       : origin = 0x00F000, length = 0x001000     /* on-chip RAM block L1 */
       ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
       FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */ 
     
    SECTIONS
    {
     
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD, 
                             RUN = RAML0, 
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL     PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
       
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : > RAML4       PAGE = 1
       data                : > RAML5       PAGE = 1
       .esysmem            : > RAMM1       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0      
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
       IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 
       FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 
             
       /* Allocate DMA-accessible RAM sections: */
       DMARAML4         : > RAML4,     PAGE = 1
       DMARAML5         : > RAML5,     PAGE = 1
       DMARAML6         : > RAML6,     PAGE = 1
       DMARAML7         : > RAML7,     PAGE = 1
       
       /* Allocate 0x400 of XINTF Zone 7 to storing data */
       ZONE7DATA        : > ZONE7B,    PAGE = 1
    
       /* .reset is a standard section used by the compiler.  It contains the */ 
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */ 
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
       
       /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
       .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD
    }
    
    SECTIONS
    {
    	Net_terminals:	> RAML4,PAGE = 1
    	Controller:		> RAML4,PAGE = 1
    	IBx_addr: 		> RAML4,PAGE = 1
    	Buck1Loop:		> RAML4,PAGE = 1
    	Buck2Loop:		> RAML4,PAGE = 1
    	DataLogTST: 	> RAML4,PAGE = 1
    	GraphData: 		> RAML4,PAGE = 1
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    

    Thanks for your help!

  • Try to change memory sections definition.

    Replace those segments:

       RAML4      : origin = 0x00C000, length = 0x001000
       RAML5      : origin = 0x00D000, length = 0x001000

    with this one:

       RAML45     : origin = 0x00C000, length = 0x002000

    And then correct ".ebss" and others' placement:

    SECTIONS
    {
       // …
       .ebss            : > RAML45,     PAGE = 1
       data              : > RAML45      PAGE = 1
       DMARAML4  : > RAML45,     PAGE = 1
       DMARAML5  : > RAML45,     PAGE = 1
       // …
    }

    SECTIONS
    {
        Net_terminals:    > RAML45,PAGE = 1
        Controller:        > RAML45,PAGE = 1
        IBx_addr:         > RAML45,PAGE = 1
        Buck1Loop:        > RAML45,PAGE = 1
        Buck2Loop:        > RAML45,PAGE = 1
        DataLogTST:     > RAML45,PAGE = 1
        GraphData:         > RAML45,PAGE = 1
    }


    > 2. Additional to the data I have, I need to declare more variables. Which memory section could I join to RAML4 and RAML5, when solved the actual problem?


    You may use RAML6 and RAML7 when you'll need more memory or want to separate data between segments.


    program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x10b0 page 1. Available memory ranges: RAML4 size: 0x1000 unused: 0x1000 max hole: 0x1000 RAML5 size: 0x1000 unused: 0x1000 max hole: 0x1000 F28335_FLASH_FlashingLeds.CMD /Prueba3 line 146 C/C++ Problem

    This error happens, cause' you can't split continious data into two memory segments even they have no gaps.

  • Hello Christian!

    You should replace all the lines that were mentioned. Changing only one line does not make sense. If you want you can send your project. Also you can try following variants:

    /*
    // TI File $Revision: /main/9 $
    // Checkin $Date: August 28, 2007   11:23:38 $
    //###########################################################################
    //
    // FILE:	F28335.cmd
    //
    // TITLE:	Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: DSP2833x Header Files V1.00 $
    // $Release Date: September 7, 2007 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file, 
    // add the header linker command file directly to the project. 
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within 
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //   
    // For BIOS applications add:      DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2833x_Headers_nonBIOS.cmd    
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the 
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper 
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
       library search path under project->build options, linker tab, 
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28335  
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
        Notes: 
              Memory blocks on F28335 are uniform (ie same
              physical memory) in both PAGE 0 and PAGE 1.  
              That is the same memory region should not be
              defined for both PAGE 0 and PAGE 1.
              Doing so will result in corruption of program 
              and/or data. 
              
              L0/L1/L2 and L3 memory blocks are mirrored - that is
              they can be accessed in high memory or low memory.
              For simplicity only one instance is used in this
              linker file. 
              
              Contiguous SARAM memory blocks can be combined 
              if required to create a larger memory block. 
     */
    
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
       RAML0123    : origin = 0x008000, length = 0x004a00     /* on-chip RAM block L0 */
       ZONE6       : origin = 0x0100000, length = 0x100000    /* XINTF zone 6 */ 
       ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 
       FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
       FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
       FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */
       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */
       FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
       FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
       FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
       OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
       ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
       
       IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
       FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML4567    : origin = 0x00Ca00, length = 0x003600     /* on-chip RAM block L1 */
       ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
       FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */ 
     
    SECTIONS
    {
     
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD, 
                             RUN = RAML0, 
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL     PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
       
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : > RAML4567    PAGE = 1
       data                : > RAML4567    PAGE = 1
       .esysmem            : > RAMM1       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0      
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
       IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 
       FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 
             
         /* Allocate DMA-accessible RAM sections: */
       DMARAML4         : > RAML4567,     PAGE = 1
       DMARAML5         : > RAML4567,     PAGE = 1
       DMARAML6         : > RAML4567,     PAGE = 1
       DMARAML7         : > RAML4567,     PAGE = 1
         
       /* Allocate 0x400 of XINTF Zone 7 to storing data */
       ZONE7DATA        : > ZONE7B,    PAGE = 1
    
       /* .reset is a standard section used by the compiler.  It contains the */ 
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */ 
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
       
       /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
       .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD
    }
    
    SECTIONS
    {
    	Net_terminals:	> RAML4567,PAGE = 1
    	Controller:		> RAML4567,PAGE = 1
    	IBx_addr: 		> RAML4567,PAGE = 1
    	Buck1Loop:		> RAML4567,PAGE = 1
    	Buck2Loop:		> RAML4567,PAGE = 1
    	DataLogTST: 	> RAML4567,PAGE = 1
    	GraphData: 		> RAML4567,PAGE = 1
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    

    /*
    // TI File $Revision: /main/9 $
    // Checkin $Date: August 28, 2007   11:23:38 $
    //###########################################################################
    //
    // FILE:	F28335.cmd
    //
    // TITLE:	Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: DSP2833x Header Files V1.00 $
    // $Release Date: September 7, 2007 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file, 
    // add the header linker command file directly to the project. 
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within 
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //   
    // For BIOS applications add:      DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2833x_Headers_nonBIOS.cmd    
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the 
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper 
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
       library search path under project->build options, linker tab, 
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28335  
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
        Notes: 
              Memory blocks on F28335 are uniform (ie same
              physical memory) in both PAGE 0 and PAGE 1.  
              That is the same memory region should not be
              defined for both PAGE 0 and PAGE 1.
              Doing so will result in corruption of program 
              and/or data. 
              
              L0/L1/L2 and L3 memory blocks are mirrored - that is
              they can be accessed in high memory or low memory.
              For simplicity only one instance is used in this
              linker file. 
              
              Contiguous SARAM memory blocks can be combined 
              if required to create a larger memory block. 
     */
    
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
       RAML0123    : origin = 0x008000, length = 0x004a00     /* on-chip RAM block L0 */
       ZONE6       : origin = 0x0100000, length = 0x100000    /* XINTF zone 6 */ 
       ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 
       FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
       FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
       FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */
       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */
       FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
       FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
       FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
       OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
       ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
       
       IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
       FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML4567    : origin = 0x00Ca00, length = 0x003600     /* on-chip RAM block L1 */
       ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
       FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */ 
     
    SECTIONS
    {
     
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD, 
                             RUN = RAML0, 
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL     PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
       
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : > RAML0123    PAGE = 0
       data                : > RAML0123    PAGE = 0
       .esysmem            : > RAMM1       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0      
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
       IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 
       FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 
             
         /* Allocate DMA-accessible RAM sections: */
       DMARAML4         : > RAML4567,     PAGE = 1
       DMARAML5         : > RAML4567,     PAGE = 1
       DMARAML6         : > RAML4567,     PAGE = 1
       DMARAML7         : > RAML4567,     PAGE = 1
         
       /* Allocate 0x400 of XINTF Zone 7 to storing data */
       ZONE7DATA        : > ZONE7B,    PAGE = 1
    
       /* .reset is a standard section used by the compiler.  It contains the */ 
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */ 
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
       
       /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
       .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD
    }
    
    SECTIONS
    {
    	Net_terminals:	> RAML4567,PAGE = 1
    	Controller:		> RAML4567,PAGE = 1
    	IBx_addr: 		> RAML4567,PAGE = 1
    	Buck1Loop:		> RAML4567,PAGE = 1
    	Buck2Loop:		> RAML4567,PAGE = 1
    	DataLogTST: 	> RAML4567,PAGE = 1
    	GraphData: 		> RAML4567,PAGE = 1
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    

    /*
    // TI File $Revision: /main/9 $
    // Checkin $Date: August 28, 2007   11:23:38 $
    //###########################################################################
    //
    // FILE:	F28335.cmd
    //
    // TITLE:	Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: DSP2833x Header Files V1.00 $
    // $Release Date: September 7, 2007 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file, 
    // add the header linker command file directly to the project. 
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within 
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //   
    // For BIOS applications add:      DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2833x_Headers_nonBIOS.cmd    
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the 
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper 
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
       library search path under project->build options, linker tab, 
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28335  
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
        Notes: 
              Memory blocks on F28335 are uniform (ie same
              physical memory) in both PAGE 0 and PAGE 1.  
              That is the same memory region should not be
              defined for both PAGE 0 and PAGE 1.
              Doing so will result in corruption of program 
              and/or data. 
              
              L0/L1/L2 and L3 memory blocks are mirrored - that is
              they can be accessed in high memory or low memory.
              For simplicity only one instance is used in this
              linker file. 
              
              Contiguous SARAM memory blocks can be combined 
              if required to create a larger memory block. 
     */
    
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
       RAML0123    : origin = 0x008000, length = 0x004a00     /* on-chip RAM block L0 */
       ZONE6       : origin = 0x0100000, length = 0x100000    /* XINTF zone 6 */ 
       ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 
       FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
       FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
       FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */
       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */
       FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
       FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
       FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
       OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
       ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
       
       IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
       FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML4567    : origin = 0x00Ca00, length = 0x003600     /* on-chip RAM block L1 */
       ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
       FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */ 
     
    SECTIONS
    {
     
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD, 
                             RUN = RAML0, 
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL     PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
       
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : > RAML4567    PAGE = 1
       data                : > RAML4567    PAGE = 1
       .esysmem            : > RAMM1       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0      
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
       IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 
       FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 
             
         /* Allocate DMA-accessible RAM sections: */
       DMARAML4         : > RAML4567,     PAGE = 1
       DMARAML5         : > RAML4567,     PAGE = 1
       DMARAML6         : > RAML4567,     PAGE = 1
       DMARAML7         : > RAML4567,     PAGE = 1
         
       /* Allocate 0x400 of XINTF Zone 7 to storing data */
       ZONE7DATA        : > ZONE7B,    PAGE = 1
    
       /* .reset is a standard section used by the compiler.  It contains the */ 
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */ 
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
       
       /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
       .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD
    }
    
    SECTIONS
    {
    	Net_terminals:	> RAML4567,PAGE = 1
    	Controller:		> RAML4567,PAGE = 1
    	IBx_addr: 		> RAML4567,PAGE = 1
    	Buck1Loop:		> RAML4567,PAGE = 1
    	Buck2Loop:		> RAML4567,PAGE = 1
    	DataLogTST: 	> RAML4567,PAGE = 1
    	GraphData: 		> RAML4567,PAGE = 1
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    
    /*
    // TI File $Revision: /main/8 $
    // Checkin $Date: June 2, 2008   11:12:24 $
    //###########################################################################
    //
    // FILE:    DSP2833x_Headers_nonBIOS.cmd
    //
    // TITLE:   DSP2833x Peripheral registers linker command file 
    //
    // DESCRIPTION: 
    // 
    //          This file is for use in Non-BIOS applications.
    //
    //          Linker command file to place the peripheral structures 
    //          used within the DSP2833x headerfiles into the correct memory
    //          mapped locations.
    //
    //          This version of the file includes the PieVectorTable structure.
    //          For BIOS applications, please use the DSP2833x_Headers_BIOS.cmd file
    //          which does not include the PieVectorTable structure.
    //
    //###########################################################################
    // $TI Release: DSP2833x/DSP2823x Header Files V1.20 $
    // $Release Date: August 1, 2008 $
    //###########################################################################
    */
    
    MEMORY
    {
     PAGE 0:    /* Program Memory */
    
     PAGE 1:    /* Data Memory */
     
       DEV_EMU     : origin = 0x000880, length = 0x000180     /* device emulation registers */
       FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */
       CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */
      
       ADC_MIRROR  : origin = 0x000B00, length = 0x000010     /* ADC Results register mirror */
    
       XINTF       : origin = 0x000B20, length = 0x000020     /* external interface registers */
       
       CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */
       CPU_TIMER1  : origin = 0x000C08, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/
       CPU_TIMER2  : origin = 0x000C10, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/
    
       PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */
       PIE_VECT    : origin = 0x000D00, length = 0x000100     /* PIE Vector Table */
    
       DMA         : origin = 0x001000, length = 0x000200     /* DMA registers */
    
       MCBSPA      : origin = 0x005000, length = 0x000040     /* McBSP-A registers */
       MCBSPB      : origin = 0x005040, length = 0x000040     /* McBSP-B registers */
    
       ECANA       : origin = 0x006000, length = 0x000040     /* eCAN-A control and status registers */ 
       ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN-A local acceptance masks */
       ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN-A message object time stamps */
       ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN-A object time-out registers */
       ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN-A mailboxes */
    
       ECANB       : origin = 0x006200, length = 0x000040     /* eCAN-B control and status registers */ 
       ECANB_LAM   : origin = 0x006240, length = 0x000040     /* eCAN-B local acceptance masks */
       ECANB_MOTS  : origin = 0x006280, length = 0x000040     /* eCAN-B message object time stamps */
       ECANB_MOTO  : origin = 0x0062C0, length = 0x000040     /* eCAN-B object time-out registers */
       ECANB_MBOX  : origin = 0x006300, length = 0x000100     /* eCAN-B mailboxes */
    
       //EPWM1       : origin = 0x006800, length = 0x000022     /* Enhanced PWM 1 registers */
       //EPWM2       : origin = 0x006840, length = 0x000022     /* Enhanced PWM 2 registers */
       //EPWM3       : origin = 0x006880, length = 0x000022     /* Enhanced PWM 3 registers */
       //EPWM4       : origin = 0x0068C0, length = 0x000022     /* Enhanced PWM 4 registers */
       //EPWM5       : origin = 0x006900, length = 0x000022     /* Enhanced PWM 5 registers */
       //EPWM6       : origin = 0x006940, length = 0x000022     /* Enhanced PWM 6 registers */
       EPWM1       : origin = 0x005800, length = 0x000022     /* Enhanced PWM 1 registers */
       EPWM2       : origin = 0x005840, length = 0x000022     /* Enhanced PWM 2 registers */
       EPWM3       : origin = 0x005880, length = 0x000022     /* Enhanced PWM 3 registers */
       EPWM4       : origin = 0x0058C0, length = 0x000022     /* Enhanced PWM 4 registers */
       EPWM5       : origin = 0x005900, length = 0x000022     /* Enhanced PWM 5 registers */
       EPWM6       : origin = 0x005940, length = 0x000022     /* Enhanced PWM 6 registers */
    
       ECAP1       : origin = 0x006A00, length = 0x000020     /* Enhanced Capture 1 registers */
       ECAP2       : origin = 0x006A20, length = 0x000020     /* Enhanced Capture 2 registers */
       ECAP3       : origin = 0x006A40, length = 0x000020     /* Enhanced Capture 3 registers */
       ECAP4       : origin = 0x006A60, length = 0x000020     /* Enhanced Capture 4 registers */         
       ECAP5       : origin = 0x006A80, length = 0x000020     /* Enhanced Capture 5 registers */         
       ECAP6       : origin = 0x006AA0, length = 0x000020     /* Enhanced Capture 6 registers */         
     
       EQEP1       : origin = 0x006B00, length = 0x000040     /* Enhanced QEP 1 registers */
       EQEP2       : origin = 0x006B40, length = 0x000040     /* Enhanced QEP 2 registers */   
    
       GPIOCTRL    : origin = 0x006F80, length = 0x000040     /* GPIO control registers */
       GPIODAT     : origin = 0x006FC0, length = 0x000020     /* GPIO data registers */
       GPIOINT     : origin = 0x006FE0, length = 0x000020     /* GPIO interrupt/LPM registers */
                     
       SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */
       SPIA        : origin = 0x007040, length = 0x000010     /* SPI-A registers */
       SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */
       XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */
    
       ADC         : origin = 0x007100, length = 0x000020     /* ADC registers */
    
       SCIB        : origin = 0x007750, length = 0x000010     /* SCI-B registers */
    
       SCIC        : origin = 0x007770, length = 0x000010     /* SCI-C registers */
       
       I2CA        : origin = 0x007900, length = 0x000040     /* I2C-A registers */
       
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */
    
       PARTID      : origin = 0x380090, length = 0x000001     /* Part ID register location */
    }
    
     
    SECTIONS
    {
       PieVectTableFile : > PIE_VECT,   PAGE = 1
    
    /*** Peripheral Frame 0 Register Structures ***/
       DevEmuRegsFile    : > DEV_EMU,     PAGE = 1
       FlashRegsFile     : > FLASH_REGS,  PAGE = 1
       CsmRegsFile       : > CSM,         PAGE = 1
       AdcMirrorFile     : > ADC_MIRROR,  PAGE = 1 
       XintfRegsFile     : > XINTF,       PAGE = 1
       CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1
       CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1
       CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1  
       PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1     
       DmaRegsFile       : > DMA,         PAGE = 1 
    
    /*** Peripheral Frame 3 Register Structures ***/
       McbspaRegsFile    : > MCBSPA,      PAGE = 1
       McbspbRegsFile    : > MCBSPB,      PAGE = 1
    
    /*** Peripheral Frame 1 Register Structures ***/
       ECanaRegsFile     : > ECANA,       PAGE = 1
       ECanaLAMRegsFile  : > ECANA_LAM    PAGE = 1   
       ECanaMboxesFile   : > ECANA_MBOX   PAGE = 1
       ECanaMOTSRegsFile : > ECANA_MOTS   PAGE = 1
       ECanaMOTORegsFile : > ECANA_MOTO   PAGE = 1
       
       ECanbRegsFile     : > ECANB,       PAGE = 1
       ECanbLAMRegsFile  : > ECANB_LAM    PAGE = 1   
       ECanbMboxesFile   : > ECANB_MBOX   PAGE = 1
       ECanbMOTSRegsFile : > ECANB_MOTS   PAGE = 1
       ECanbMOTORegsFile : > ECANB_MOTO   PAGE = 1
       
       EPwm1RegsFile     : > EPWM1        PAGE = 1   
       EPwm2RegsFile     : > EPWM2        PAGE = 1   
       EPwm3RegsFile     : > EPWM3        PAGE = 1   
       EPwm4RegsFile     : > EPWM4        PAGE = 1   
       EPwm5RegsFile     : > EPWM5        PAGE = 1   
       EPwm6RegsFile     : > EPWM6        PAGE = 1
       
       ECap1RegsFile     : > ECAP1        PAGE = 1   
       ECap2RegsFile     : > ECAP2        PAGE = 1   
       ECap3RegsFile     : > ECAP3        PAGE = 1   
       ECap4RegsFile     : > ECAP4        PAGE = 1
       ECap5RegsFile     : > ECAP5        PAGE = 1   
       ECap6RegsFile     : > ECAP6        PAGE = 1
    
       EQep1RegsFile     : > EQEP1        PAGE = 1   
       EQep2RegsFile     : > EQEP2        PAGE = 1               
    
       GpioCtrlRegsFile  : > GPIOCTRL     PAGE = 1
       GpioDataRegsFile  : > GPIODAT      PAGE = 1
       GpioIntRegsFile   : > GPIOINT      PAGE = 1
       
    /*** Peripheral Frame 2 Register Structures ***/
       SysCtrlRegsFile   : > SYSTEM,      PAGE = 1
       SpiaRegsFile      : > SPIA,        PAGE = 1
       SciaRegsFile      : > SCIA,        PAGE = 1
       XIntruptRegsFile  : > XINTRUPT,    PAGE = 1
       AdcRegsFile       : > ADC,         PAGE = 1
       ScibRegsFile      : > SCIB,        PAGE = 1
       ScicRegsFile      : > SCIC,        PAGE = 1
       I2caRegsFile      : > I2CA,        PAGE = 1
                  
    /*** Code Security Module Register Structures ***/
       CsmPwlFile        : > CSM_PWL,     PAGE = 1
    
    /*** Device Part ID Register Structures ***/
       PartIdRegsFile    : > PARTID,      PAGE = 1
    
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

    /*
    // TI File $Revision: /main/9 $
    // Checkin $Date: August 28, 2007   11:23:38 $
    //###########################################################################
    //
    // FILE:	F28335.cmd
    //
    // TITLE:	Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: DSP2833x Header Files V1.00 $
    // $Release Date: September 7, 2007 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file, 
    // add the header linker command file directly to the project. 
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within 
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //   
    // For BIOS applications add:      DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2833x_Headers_nonBIOS.cmd    
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the 
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper 
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
       library search path under project->build options, linker tab, 
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28335  
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
        Notes: 
              Memory blocks on F28335 are uniform (ie same
              physical memory) in both PAGE 0 and PAGE 1.  
              That is the same memory region should not be
              defined for both PAGE 0 and PAGE 1.
              Doing so will result in corruption of program 
              and/or data. 
              
              L0/L1/L2 and L3 memory blocks are mirrored - that is
              they can be accessed in high memory or low memory.
              For simplicity only one instance is used in this
              linker file. 
              
              Contiguous SARAM memory blocks can be combined 
              if required to create a larger memory block. 
     */
    
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
       RAML0123    : origin = 0x008000, length = 0x004a00     /* on-chip RAM block L0 */
       ZONE6       : origin = 0x0100000, length = 0x100000    /* XINTF zone 6 */ 
       ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 
       FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
       FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
       FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */
       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */
       FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
       FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
       FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
       OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
       ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
       
       IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
       FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML4567    : origin = 0x00Ca00, length = 0x003600     /* on-chip RAM block L1 */
       ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
       FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */ 
     
    SECTIONS
    {
     
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD, 
                             RUN = RAML0, 
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL     PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
       
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : > RAML0123    PAGE = 0
       data                : > RAML0123    PAGE = 0
       .esysmem            : > RAMM1       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0      
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
       IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 
       FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 
             
         /* Allocate DMA-accessible RAM sections: */
       DMARAML4         : > RAML4567,     PAGE = 1
       DMARAML5         : > RAML4567,     PAGE = 1
       DMARAML6         : > RAML4567,     PAGE = 1
       DMARAML7         : > RAML4567,     PAGE = 1
         
       /* Allocate 0x400 of XINTF Zone 7 to storing data */
       ZONE7DATA        : > ZONE7B,    PAGE = 1
    
       /* .reset is a standard section used by the compiler.  It contains the */ 
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */ 
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
       
       /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
       .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD
    }
    
    SECTIONS
    {
    	Net_terminals:	> RAML4567,PAGE = 1
    	Controller:		> RAML4567,PAGE = 1
    	IBx_addr: 		> RAML4567,PAGE = 1
    	Buck1Loop:		> RAML4567,PAGE = 1
    	Buck2Loop:		> RAML4567,PAGE = 1
    	DataLogTST: 	> RAML4567,PAGE = 1
    	GraphData: 		> RAML4567,PAGE = 1
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    
    /*
    // TI File $Revision: /main/8 $
    // Checkin $Date: June 2, 2008   11:12:24 $
    //###########################################################################
    //
    // FILE:    DSP2833x_Headers_nonBIOS.cmd
    //
    // TITLE:   DSP2833x Peripheral registers linker command file 
    //
    // DESCRIPTION: 
    // 
    //          This file is for use in Non-BIOS applications.
    //
    //          Linker command file to place the peripheral structures 
    //          used within the DSP2833x headerfiles into the correct memory
    //          mapped locations.
    //
    //          This version of the file includes the PieVectorTable structure.
    //          For BIOS applications, please use the DSP2833x_Headers_BIOS.cmd file
    //          which does not include the PieVectorTable structure.
    //
    //###########################################################################
    // $TI Release: DSP2833x/DSP2823x Header Files V1.20 $
    // $Release Date: August 1, 2008 $
    //###########################################################################
    */
    
    MEMORY
    {
     PAGE 0:    /* Program Memory */
    
     PAGE 1:    /* Data Memory */
     
       DEV_EMU     : origin = 0x000880, length = 0x000180     /* device emulation registers */
       FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */
       CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */
      
       ADC_MIRROR  : origin = 0x000B00, length = 0x000010     /* ADC Results register mirror */
    
       XINTF       : origin = 0x000B20, length = 0x000020     /* external interface registers */
       
       CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */
       CPU_TIMER1  : origin = 0x000C08, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/
       CPU_TIMER2  : origin = 0x000C10, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/
    
       PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */
       PIE_VECT    : origin = 0x000D00, length = 0x000100     /* PIE Vector Table */
    
       DMA         : origin = 0x001000, length = 0x000200     /* DMA registers */
    
       MCBSPA      : origin = 0x005000, length = 0x000040     /* McBSP-A registers */
       MCBSPB      : origin = 0x005040, length = 0x000040     /* McBSP-B registers */
    
       ECANA       : origin = 0x006000, length = 0x000040     /* eCAN-A control and status registers */ 
       ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN-A local acceptance masks */
       ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN-A message object time stamps */
       ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN-A object time-out registers */
       ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN-A mailboxes */
    
       ECANB       : origin = 0x006200, length = 0x000040     /* eCAN-B control and status registers */ 
       ECANB_LAM   : origin = 0x006240, length = 0x000040     /* eCAN-B local acceptance masks */
       ECANB_MOTS  : origin = 0x006280, length = 0x000040     /* eCAN-B message object time stamps */
       ECANB_MOTO  : origin = 0x0062C0, length = 0x000040     /* eCAN-B object time-out registers */
       ECANB_MBOX  : origin = 0x006300, length = 0x000100     /* eCAN-B mailboxes */
    
       //EPWM1       : origin = 0x006800, length = 0x000022     /* Enhanced PWM 1 registers */
       //EPWM2       : origin = 0x006840, length = 0x000022     /* Enhanced PWM 2 registers */
       //EPWM3       : origin = 0x006880, length = 0x000022     /* Enhanced PWM 3 registers */
       //EPWM4       : origin = 0x0068C0, length = 0x000022     /* Enhanced PWM 4 registers */
       //EPWM5       : origin = 0x006900, length = 0x000022     /* Enhanced PWM 5 registers */
       //EPWM6       : origin = 0x006940, length = 0x000022     /* Enhanced PWM 6 registers */
       EPWM1       : origin = 0x005800, length = 0x000022     /* Enhanced PWM 1 registers */
       EPWM2       : origin = 0x005840, length = 0x000022     /* Enhanced PWM 2 registers */
       EPWM3       : origin = 0x005880, length = 0x000022     /* Enhanced PWM 3 registers */
       EPWM4       : origin = 0x0058C0, length = 0x000022     /* Enhanced PWM 4 registers */
       EPWM5       : origin = 0x005900, length = 0x000022     /* Enhanced PWM 5 registers */
       EPWM6       : origin = 0x005940, length = 0x000022     /* Enhanced PWM 6 registers */
    
       ECAP1       : origin = 0x006A00, length = 0x000020     /* Enhanced Capture 1 registers */
       ECAP2       : origin = 0x006A20, length = 0x000020     /* Enhanced Capture 2 registers */
       ECAP3       : origin = 0x006A40, length = 0x000020     /* Enhanced Capture 3 registers */
       ECAP4       : origin = 0x006A60, length = 0x000020     /* Enhanced Capture 4 registers */         
       ECAP5       : origin = 0x006A80, length = 0x000020     /* Enhanced Capture 5 registers */         
       ECAP6       : origin = 0x006AA0, length = 0x000020     /* Enhanced Capture 6 registers */         
     
       EQEP1       : origin = 0x006B00, length = 0x000040     /* Enhanced QEP 1 registers */
       EQEP2       : origin = 0x006B40, length = 0x000040     /* Enhanced QEP 2 registers */   
    
       GPIOCTRL    : origin = 0x006F80, length = 0x000040     /* GPIO control registers */
       GPIODAT     : origin = 0x006FC0, length = 0x000020     /* GPIO data registers */
       GPIOINT     : origin = 0x006FE0, length = 0x000020     /* GPIO interrupt/LPM registers */
                     
       SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */
       SPIA        : origin = 0x007040, length = 0x000010     /* SPI-A registers */
       SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */
       XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */
    
       ADC         : origin = 0x007100, length = 0x000020     /* ADC registers */
    
       SCIB        : origin = 0x007750, length = 0x000010     /* SCI-B registers */
    
       SCIC        : origin = 0x007770, length = 0x000010     /* SCI-C registers */
       
       I2CA        : origin = 0x007900, length = 0x000040     /* I2C-A registers */
       
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */
    
       PARTID      : origin = 0x380090, length = 0x000001     /* Part ID register location */
    }
    
     
    SECTIONS
    {
       PieVectTableFile : > PIE_VECT,   PAGE = 1
    
    /*** Peripheral Frame 0 Register Structures ***/
       DevEmuRegsFile    : > DEV_EMU,     PAGE = 1
       FlashRegsFile     : > FLASH_REGS,  PAGE = 1
       CsmRegsFile       : > CSM,         PAGE = 1
       AdcMirrorFile     : > ADC_MIRROR,  PAGE = 1 
       XintfRegsFile     : > XINTF,       PAGE = 1
       CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1
       CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1
       CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1  
       PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1     
       DmaRegsFile       : > DMA,         PAGE = 1 
    
    /*** Peripheral Frame 3 Register Structures ***/
       McbspaRegsFile    : > MCBSPA,      PAGE = 1
       McbspbRegsFile    : > MCBSPB,      PAGE = 1
    
    /*** Peripheral Frame 1 Register Structures ***/
       ECanaRegsFile     : > ECANA,       PAGE = 1
       ECanaLAMRegsFile  : > ECANA_LAM    PAGE = 1   
       ECanaMboxesFile   : > ECANA_MBOX   PAGE = 1
       ECanaMOTSRegsFile : > ECANA_MOTS   PAGE = 1
       ECanaMOTORegsFile : > ECANA_MOTO   PAGE = 1
       
       ECanbRegsFile     : > ECANB,       PAGE = 1
       ECanbLAMRegsFile  : > ECANB_LAM    PAGE = 1   
       ECanbMboxesFile   : > ECANB_MBOX   PAGE = 1
       ECanbMOTSRegsFile : > ECANB_MOTS   PAGE = 1
       ECanbMOTORegsFile : > ECANB_MOTO   PAGE = 1
       
       EPwm1RegsFile     : > EPWM1        PAGE = 1   
       EPwm2RegsFile     : > EPWM2        PAGE = 1   
       EPwm3RegsFile     : > EPWM3        PAGE = 1   
       EPwm4RegsFile     : > EPWM4        PAGE = 1   
       EPwm5RegsFile     : > EPWM5        PAGE = 1   
       EPwm6RegsFile     : > EPWM6        PAGE = 1
       
       ECap1RegsFile     : > ECAP1        PAGE = 1   
       ECap2RegsFile     : > ECAP2        PAGE = 1   
       ECap3RegsFile     : > ECAP3        PAGE = 1   
       ECap4RegsFile     : > ECAP4        PAGE = 1
       ECap5RegsFile     : > ECAP5        PAGE = 1   
       ECap6RegsFile     : > ECAP6        PAGE = 1
    
       EQep1RegsFile     : > EQEP1        PAGE = 1   
       EQep2RegsFile     : > EQEP2        PAGE = 1               
    
       GpioCtrlRegsFile  : > GPIOCTRL     PAGE = 1
       GpioDataRegsFile  : > GPIODAT      PAGE = 1
       GpioIntRegsFile   : > GPIOINT      PAGE = 1
       
    /*** Peripheral Frame 2 Register Structures ***/
       SysCtrlRegsFile   : > SYSTEM,      PAGE = 1
       SpiaRegsFile      : > SPIA,        PAGE = 1
       SciaRegsFile      : > SCIA,        PAGE = 1
       XIntruptRegsFile  : > XINTRUPT,    PAGE = 1
       AdcRegsFile       : > ADC,         PAGE = 1
       ScibRegsFile      : > SCIB,        PAGE = 1
       ScicRegsFile      : > SCIC,        PAGE = 1
       I2caRegsFile      : > I2CA,        PAGE = 1
                  
    /*** Code Security Module Register Structures ***/
       CsmPwlFile        : > CSM_PWL,     PAGE = 1
    
    /*** Device Part ID Register Structures ***/
       PartIdRegsFile    : > PARTID,      PAGE = 1
    
    }
    
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

    Regards,

    Igor

  • BTW, you may try to correct a little bit a previous statement before changing a number of lines:

        .ebss : >> RAML4 | RAML5   PAGE = 1

    The ">>" operator used to indicate that an output section can be split into specified memory ranges, spru513e.pdf, p.195, 7.5.4.7.

  • Thanks to both of you! I finally changed the memory section lengths, and it worked fine.

    I will also review the variants you sent me, and the use of  ">>" operator.