Other Parts Discussed in Thread: INSTASPIN-BLDC, CONTROLSUITE, CCSTUDIO
Hello,
I am trying to drive a +12V motor with the DRV8312-C2-KIT_v128 InstaSPIN_BLDC development kit and I am unable. When driving a +24V motor, and lowering the voltage very slowly, the board seems to cut out at +19V. When I say cut out I mean that the motor just stops and the power supply even current limits. Even though the current draw was not even 10% of the limit. I have determined that this is not a supply issue but a micro controller threshold issue.
Is it possible in this kit to drive a +12V motor?
Thank you,
Matt