Hi experts.
I'm trying to connect HV_SOLAR_DC_AC (TMDSHV1PHINVKIT) EVM with SD XDS560v2 and C2803xHWdevPkg(not ISO).
When "Test Connection" on CCSv5 it shows error as below
Error connecting to the target:
Error 0x80000240/-233
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.
SC_ERR_PATH_BROKEN <-233>
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
Jumper placed on JP6 and manual don't refer to anything with external emulator. I couldn't find any reason why it does not work.
The combination of Experimenter kits with XDS560v2 and C28035 control card works fine.
Please give some check point.
Best regards.
Jay.