This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

get c_int00 address in c-code

Hi,

I need the c_int00 in c-code.

What I want is to store the entry point to a specific location so, my program can be started from another application inside the same EEprom.

I tried to do it in Assembler like:

;---------------------------------------------------------------------
    .ref _c_int00

    .sect "BootloaderStartAddr"

BootloaderStartAddr:
        .long _c_int00         ;Branch to start of boot.asm in RTS library

;---------------------------------------------------------------------

so what I want to do is:


extern long c_int00;
#pragma DATA_SECTION(usBootloaderStartAddr, "BootloaderStartAddr")
const long usBootloaderStartAddr                 = c_int00;

but then the complier gives the following warning:

#28 expression must have a constant value

how do I get the c_int00 in C-Code or at least at compile time?

Thanks in advance

Heiny