Other Parts Discussed in Thread: DRV8301, DRV8312
Hello,
I want to bay the DRV 8301 ore the 8312 kit to lurn to program and use it for the existing high part (MOSFET'S) of my old controllers now. Though these controllers can switch 72 to 90 V and 500 A, this is probably possible to overcome bud these controllers can also ore have the regenerate / brake option to deliver the kinetic energy back to the battery block. In the controllers is used the sdPIC33FJ64MC706A from microchip now, bud they don't have this nice and easy programming software.
I haven't seen this brake / regeneration option mentioned in the different video's ore the pdf's of TI kit's. Do they have this option ore not and can the speed of the motors also be controlled via the now existing signal that comes from the throttle pedal. The motors are used in an electric car conversion.
Can somebody help me ?
Thanks in advance,
D.