Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
Hi all..
My friend's TMS320F28335 docking station is getting heated up whenever it is connected to pc.
When it is connected to pc it also shows an error message :'surge rush current'.
The resistance between vcc and ground is just 1.2ohms.
I checked the same resistance after removing the tms320f28335 control card,it was showing 1.2ohms again. I'm sure that problem is only with docking station.not with control card.
Once accidentally ground pin of f28335 has been connected to different potential. That might be the reason for this.
What can be done for this?Can i repair the docking station myself?
Is warranty applicable for this?If i want to buy a new one,docking station alone is available for sale?
Please answer my queries...
thanks®ards
Mahesh