I am developing on the F2808 device on the C2000 docking station. The F2808 Data Manual (SPRS230N rev May 2012, p. 35) indicates that the "Boot to Flash" mode requires pins GPIO18, 29, and 34 to be set to 1's. However, when I jumpered the pins to 1, I wasn't able to "boot to flash" -- I was able to "boot to flash" with pins unjumpered. I interpret this as setting the pins to 0's which is opposite of what was specified in the data manual.
The schematic of my Docking Station (CC28xxx Docking Station Rel-2, Rev A) appears to be outdated. This is because the header "pin #1" on the board is HI at (3.3V, which is expected); conversely, the Rev A schematic shows pin #1 grounded through a 20MOhm resistor.
Am I interpreting the datasheet correctly? Where can I find updated versions of the F2808 datasheet and Docking Station schematic that is consistent with my setup (F2808 Docking Station USB-EMU [R3])?