Other Parts Discussed in Thread: CONTROLSUITE
Hi everyone,
I've got a stupid question, but it's necessary for me to know the answer : where do i need to put jumper to operate the uart-echo example which is on the controlSUITE ?
Regards,
Sébastien.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
Hi everyone,
I've got a stupid question, but it's necessary for me to know the answer : where do i need to put jumper to operate the uart-echo example which is on the controlSUITE ?
Regards,
Sébastien.
Hello Sébastien!
I see you have some problems. I don't remember what is the name of your KIT (docking station). Where is your jumper (it is on controlCARD or on main board)? Enter please at the title of your post the name of your KIT based on F28M35. This will provide you the better support, because community members will understand better what kind of device in question.
Regards,
Igor
Hi Igor,
My H52C1 Concerto Experimenter Kit is "TMDXDOCKH52C1" , and my jumper is on my main board.
Thanks for your patience Igor.
Regards,
Sébastien.
Sebastien,
The Concerto F28M35H52C1 controlCARD connects to a computer via the mini-USB connector on the controlCARD itself. This USB connection can transmit both JTAG connectivity and UART.
In order to get the example working you should need to connect a mini-USB cable between the computer and the controlCARD. You also need to make sure that SW3 is properly configured. Then hyperterminal or some client on the PC will transmit and receive the echoed data.
The infosheet and schematics should help you understand the hardware. These are available in controlSUITE at the below:
\controlSUITE\development_kits\~controlCARDs\CCF28M35xxHWdevPkg_v2\
Thank you,
Brett