Dear All
Just i have connected dsp borad in host pc via USB port .. When i tried to open CCS V3 , it showed the following error meassage
I/O Port=540
Borad name: F28335_eZdsp
Cpu Name:CPU_0
What are the solutions ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All
Just i have connected dsp borad in host pc via USB port .. When i tried to open CCS V3 , it showed the following error meassage
I/O Port=540
Borad name: F28335_eZdsp
Cpu Name:CPU_0
What are the solutions ?
Hi!
First of all. Did you install the USB-connection driver for your F28335_eZdsp? Have this driver been installed correctly? Attach your device to USB of PC and power-on device. Look at the System device maneger of PC. Find your new USB-connection. If you can not find it then try reinstall driver.
Regards,
Igor
I have installed eZdsp28335 Drivers and Target Content from TI CD including CCS V3.3
Same problem
Hi!
What did you install the first: CCS or eZdsp28335 Drivers? Try uninstall all. Install CCS furst and then eZdsp28335 Drivers.
Regards,
Igor
I did it ..but it has showed the same problem ...
Let make it clear :
I have only connected USB cable to PC from DSP board nothing else ..after switching power on dsp board
is it ok?
Hi!
Did you try to find your target device USB-connection at System device manager of PC when the target device power-on?
Regards,
Igor