Other Parts Discussed in Thread: CONTROLSUITE
There is a bug in the new enet_uip example. Please replace the enet_uip.c source file with the one attached in this discussion.
//###########################################################################
// FILE: enet_uip.c
// TITLE: Ethernet GPIO control using uIP TCP/IP stack
//###########################################################################
// $TI Release: F28M35x Support Library v201 $
// $Release Date: Fri Jun 7 10:51:13 CDT 2013 $
//###########################################################################
#include "inc/hw_ints.h"
#include "inc/hw_nvic.h"
#include "inc/hw_gpio.h"
#include "inc/hw_udma.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_ethernet.h"
#include "board_drivers/set_pinout_f28m35x.h"
#include "driverlib/udma.h"
#include "driverlib/gpio.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/ethernet.h"
#include "driverlib/interrupt.h"
#include "utils/ustdlib.h"
#include "utils/uartstdio.h"
#include "uip/uip.h"
#include "uip/uip_arp.h"
#include "httpd.h"
#include "dhcpc/dhcpc.h"
//*****************************************************************************
//! \addtogroup master_example_list
//! <h1>Ethernet GPIO control using uIP stack (enet_uip)</h1>
//!
//! This example application demonstrates controlling a GPIO pin using ethernet
//! communication. It makes use of the uIP TCP/IP stack.
//! A basic web site is served over the Ethernet port. The web site displays
//! a few lines of text, a Toggle LED button, an input to select an LED (6 or 7)
//! and a get status button. The user specifies which LED needs to be toggled
//! and presses the Toggle button. The user gets the status of the LED(ON or
//! OFF), by pressing the Get status button.
//! This code uses a static IP address. Depending on the client machine,the user
//! may need to manually set a fixed static IP address.
//! Follow the following steps to assign a static IP address to the client
//! machine
//! - disable any wireless connection that may be active.
//! - start-> control Panel->right click on "Network connection"->open.
//! - Identify the connection to use "Local Area connection" or "Wired
//! Network Connection" or some other name depending on the client machine.
//! - Right click on the connection -> click on properties. In the "Local Area
//! Connection" or "Wired Network connection" properties window under
//! "general" tab in the "This connection uses the following items:" list
//! scroll down and click on "Internet Protocol (TCP/IP)" item(! don't
//! uncheck it). click on properties. In the "Internet Protocol(TCP/IP)
//! properties" window select "Use the following IP address" and enter the
//! following:
//! IP address: "169.254.42.86"
//! Subnet mask: "255.255.0.0"
//! - click "ok" twice to close the open dialog boxes.
//! - Remember to revert back the above settings to their default values once
//! the use of this server is complete.
//! - The IP address for the server is "169.254.254.169"
//!
//!
//! \b Note
//! - Connect the MAC with the PHY using the provided jumpers.
//! Connect the first 15 pins of Row C to Row B using the jumpers.
//!
//! - All EMAC examples use a generic TI�s MAC address A8-63-F2-00-00-80.
//! User defined MAC address can be programmed in a fixed non-volatile memory
//! location. Refer to device data sheet and reference guides for details.
//!
//! \b Caution
//! - If you have two concerto CCARDS communicating with each other, they
//! need to have different EMAC addresses.
//!
//! For additional details on uIP, refer to the uIP web page at:
//! http://www.sics.se/~adam/old-uip/
//
//*****************************************************************************
//*****************************************************************************
// Defines for setting up the system clock.
//*****************************************************************************
#define SYSTICKHZ CLOCK_CONF_SECOND
#define SYSTICKMS (1000 / SYSTICKHZ)
#define SYSTICKUS (1000000 / SYSTICKHZ)
#define SYSTICKNS (1000000000 / SYSTICKHZ)
//*****************************************************************************
// Macro for accessing the Ethernet header information in the buffer.
//*****************************************************************************
u8_t ucUIPBuffer[UIP_BUFSIZE + 2];
u8_t *uip_buf;
#define BUF ((struct uip_eth_hdr *)uip_buf)
//*****************************************************************************
// A set of flags. The flag bits are defined as follows:
// 0 -> An indicator that a SysTick interrupt has occurred.
// 1 -> An RX Packet has been received.
// 2 -> A TX packet DMA transfer is pending.
// 3 -> A RX packet DMA transfer is pending.
//*****************************************************************************
#define FLAG_SYSTICK 0
#define FLAG_RXPKT 1
#define FLAG_TXPKT 2
#define FLAG_RXPKTPEND 3
static volatile unsigned long g_ulFlags;
//*****************************************************************************
// A system tick counter, incremented every SYSTICKMS.
//*****************************************************************************
volatile unsigned long g_ulTickCounter = 0;
//*****************************************************************************
// The control table used by the uDMA controller. This table must be aligned
// to a 1024 byte boundary. In this application uDMA is only used for USB,
// so only the first 8 channels are needed.
//*****************************************************************************
#pragma DATA_ALIGN(g_sDMAControlTable, 1024)
tDMAControlTable g_sDMAControlTable[8];
//*****************************************************************************
// Default TCP/IP Settings for this application.
// Default to Link Local address ... (169.254.1.0 to 169.254.254.255). Note:
// This application does not implement the Zeroconf protocol. No ARP query is
// issued to determine if this static IP address is already in use.
// TODO: Uncomment the following #define statement to enable STATIC IP
// instead of DHCP.
//*****************************************************************************
#define USE_STATIC_IP
#ifndef DEFAULT_IPADDR0
#define DEFAULT_IPADDR0 169
#endif
#ifndef DEFAULT_IPADDR1
#define DEFAULT_IPADDR1 254
#endif
#ifndef DEFAULT_IPADDR2
#define DEFAULT_IPADDR2 254
#endif
#ifndef DEFAULT_IPADDR3
#define DEFAULT_IPADDR3 169
#endif
#ifndef DEFAULT_NETMASK0
#define DEFAULT_NETMASK0 255
#endif
#ifndef DEFAULT_NETMASK1
#define DEFAULT_NETMASK1 255
#endif
#ifndef DEFAULT_NETMASK2
#define DEFAULT_NETMASK2 0
#endif
#ifndef DEFAULT_NETMASK3
#define DEFAULT_NETMASK3 0
#endif
//*****************************************************************************
// UIP Timers (in MS)
//*****************************************************************************
#define UIP_PERIODIC_TIMER_MS 500
#define UIP_ARP_TIMER_MS 10000
//*****************************************************************************
// Defines for commands
//*****************************************************************************
#define TOGGLE_LED_6 0xA1
#define TOGGLE_LED_7 0xA2
#define GET_LED6_STATUS 0xA3
#define GET_LED7_STATUS 0xA4
#define INVALID_CMD 0xA5
#define INVALID_INPUT 0xA6
#define NO_CMD 0xA6
//*****************************************************************************
// functions added in httpd.c
//*****************************************************************************
extern void httpd_clear_command(void);
extern void httpd_clear_command(void);
extern int httpd_get_command(int *command_word);
extern void httpd_insert_response(int data_length,char *data);
//*****************************************************************************
// Responses displayed to the user
//*****************************************************************************
const char led6_on[] = " LED6_ON";
const char led6_off[] = "LED6_OFF";
const char led7_on[] = " LED7_ON";
const char led7_off[] = "LED7_OFF";
//*****************************************************************************
// The error routine that is called if the driver library encounters an error.
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
//*****************************************************************************
// The interrupt handler for the SysTick interrupt.
//*****************************************************************************
void
SysTickIntHandler(void)
{
// Increment the system tick count.
g_ulTickCounter++;
// Indicate that a SysTick interrupt has occurred.
HWREGBITW(&g_ulFlags, FLAG_SYSTICK) = 1;
}
//*****************************************************************************
// Display the current IP address on the screen and transmit it via the UART.
//*****************************************************************************
void
ShowIPAddress(const uip_ipaddr_t sIPAddr)
{
char pcBuffer[24];
usprintf(pcBuffer, "IP: %d.%d.%d.%d", sIPAddr[0] & 0xff,
sIPAddr[0] >> 8, sIPAddr[1] & 0xff, sIPAddr[1] >> 8);
}
//*****************************************************************************
//! When using the timer module in UIP, this function is required to return
//! the number of ticks. Note that the file "clock-arch.h" must be provided
//! by the application, and define CLOCK_CONF_SECONDS as the number of ticks
//! per second, and must also define the typedef "clock_time_t".
//*****************************************************************************
clock_time_t
clock_time(void)
{
return((clock_time_t)g_ulTickCounter);
}
//*****************************************************************************
// The interrupt handler for the Ethernet interrupt.
//*****************************************************************************
void
EthernetIntHandler(void)
{
unsigned long ulTemp;
// Read and Clear the interrupt.
ulTemp = EthernetIntStatus(ETH_BASE, false);
EthernetIntClear(ETH_BASE, ulTemp);
// Check to see if an RX Interrupt has occurred.
if(ulTemp & ETH_INT_RX)
{
// Indicate that a packet has been received.
HWREGBITW(&g_ulFlags, FLAG_RXPKT) = 1;
// Disable Ethernet RX Interrupt.
EthernetIntDisable(ETH_BASE, ETH_INT_RX);
}
// Check to see if waiting on a DMA to complete.
if(HWREGBITW(&g_ulFlags, FLAG_RXPKTPEND) == 1)
{
// Verify the channel transfer is done
if(uDMAChannelModeGet(UDMA_CHANNEL_ETH0RX) == UDMA_MODE_STOP)
{
// Indicate that a data has been read in.
HWREGBITW(&g_ulFlags, FLAG_RXPKTPEND) = 0;
}
}
// Check to see if the Ethernet TX uDMA channel was pending.
if(HWREGBITW(&g_ulFlags, FLAG_TXPKT) == 1)
{
// Verify the channel transfer is done
if(uDMAChannelModeGet(UDMA_CHANNEL_ETH0TX) == UDMA_MODE_STOP)
{
// Trigger the transmission of the data.
HWREG(ETH_BASE + MAC_O_TR) = MAC_TR_NEWTX;
// Indicate that a packet has been sent.
HWREGBITW(&g_ulFlags, FLAG_TXPKT) = 0;
}
}
}
//*****************************************************************************
// Callback for when DHCP client has been configured.
//*****************************************************************************
void
dhcpc_configured(const struct dhcpc_state *s)
{
uip_sethostaddr(&s->ipaddr);
uip_setnetmask(&s->netmask);
uip_setdraddr(&s->default_router);
ShowIPAddress(s->ipaddr);
}
//*****************************************************************************
// Read a packet using DMA instead of directly reading the FIFO if the
// alignment will allow it.
//*****************************************************************************
long
EthernetPacketGetDMA(unsigned long ulBase, unsigned char *pucBuf, long lBufLen)
{
unsigned long ulTemp;
unsigned char pucData[4];
unsigned char *pucBuffer;
long lTempLen, lFrameLen;
long lRemainder;
int iIdx;
// Check the arguments.
ASSERT(ulBase == ETH_BASE);
ASSERT(pucBuf != 0);
ASSERT(lBufLen > 0);
// If the buffer is not aligned on an odd half-word then it cannot use DMA.
// This is because the two packet length bytes are written in front of the
// packet, and the packet data must have two bytes that can be pulled off
// to become a word and leave the remainder of the buffer word aligned.
if(((unsigned long)pucBuf & 3) != 2)
{
// If there is not proper alignment the packet must be sent without
// using DMA.
return(EthernetPacketGetNonBlocking(ulBase, pucBuf, lBufLen));
}
// Read WORD 0 from the FIFO, set the receive Frame Length and store the
// first two bytes of the destination address in the receive buffer.
ulTemp = HWREG(ulBase + MAC_O_DATA);
lFrameLen = (long)(ulTemp & 0xffff);
pucBuf[0] = (unsigned char)((ulTemp >> 16) & 0xff);
pucBuf[1] = (unsigned char)((ulTemp >> 24) & 0xff);
// The maximum DMA size is the frame size - the two bytes already read and
// truncated to the nearest word size.
lTempLen = (lFrameLen - 2) & 0xfffffffc;
lRemainder = (lFrameLen - 2) & 3;
// Don't allow writing beyond the end of the buffer.
if(lBufLen < lTempLen)
{
lRemainder = lTempLen - lBufLen;
lTempLen = lBufLen;
}
else if(lBufLen >= (lFrameLen - 2 + 3))
{
// If there is room, just DMA the last word as well so that the
// special copy after DMA is not required.
lRemainder = 0;
lTempLen = lFrameLen - 2 + 3;
}
// Mark the receive as pending.
HWREGBITW(&g_ulFlags, FLAG_RXPKTPEND) = 1;
// Set up the DMA to transfer the Ethernet header when a
// packet is received
uDMAChannelTransferSet(UDMA_CHANNEL_ETH0RX, UDMA_MODE_AUTO,
(void *)(ETH_BASE + MAC_O_DATA),
&pucBuf[2], lTempLen>>2);
uDMAChannelEnable(UDMA_CHANNEL_ETH0RX);
// Issue a software request to start the channel running.
uDMAChannelRequest(UDMA_CHANNEL_ETH0RX);
// Wait for the previous transmission to be complete.
while(HWREGBITW(&g_ulFlags, FLAG_RXPKTPEND) == 1)
{
}
// See if there are extra bytes to read into the buffer.
if(lRemainder)
{
// If the remainder is more than 3 bytes then the buffer was never big
// enough and data must be tossed.
if(lRemainder > 3)
{
// Read any remaining WORDS (that did not fit into the buffer).
while(lRemainder > 0)
{
ulTemp = HWREG(ulBase + MAC_O_DATA);
lRemainder -= 4;
}
}
// Read the last word from the FIFO.
*((unsigned long *)&pucData[0]) = HWREG(ulBase + MAC_O_DATA);
// The current buffer position is lTempLen plus the two bytes read
// from the first word.
pucBuffer = &pucBuf[lTempLen + 2];
// Read off each individual byte and save it.
for(iIdx = 0; iIdx < lRemainder; iIdx++)
{
pucBuffer[iIdx] = pucData[iIdx];
}
}
// If frame was larger than the buffer, return the "negative" frame length.
lFrameLen -= 6;
if(lFrameLen > lBufLen)
{
return(-lFrameLen);
}
// Return the Frame Length
return(lFrameLen);
}
//*****************************************************************************
// Transmit a packet using DMA instead of directly writing the FIFO if the
// alignment will allow it.
//*****************************************************************************
static long
EthernetPacketPutDMA(unsigned long ulBase, unsigned char *pucBuf,
long lBufLen)
{
unsigned long ulTemp;
// If the buffer is not aligned on an odd half-word then it cannot use DMA.
// This is because the two packet length bytes are written in front of the
// packet, and the packet data must have two bytes that can be pulled off
// to become a word and leave the remainder of the buffer word aligned.
if(((unsigned long)pucBuf & 3) != 2)
{
// If there is not proper aligment the packet must be sent without
// using DMA.
return(EthernetPacketPut(ulBase, pucBuf, lBufLen));
}
// Indicate that a packet is being sent.
HWREGBITW(&g_ulFlags, FLAG_TXPKT) = 1;
// Build and write WORD 0 (see format above) to the transmit FIFO.
ulTemp = (unsigned long)(lBufLen - 14);
ulTemp |= (*pucBuf++) << 16;
ulTemp |= (*pucBuf++) << 24;
HWREG(ulBase + MAC_O_DATA) = ulTemp;
// Force an extra word to be transferred if the end of the buffer is not
// aligned on a word boundary. The math is actually lBufLen - 2 + 3 to
// insure that the proper number of bytes are written.
lBufLen += 1;
// Configure the TX DMA channel to transfer the packet buffer.
uDMAChannelTransferSet(UDMA_CHANNEL_ETH0TX, UDMA_MODE_AUTO,
pucBuf, (void *)(ETH_BASE + MAC_O_DATA),
lBufLen>>2);
// Enable the Ethernet Transmit DMA channel.
uDMAChannelEnable(UDMA_CHANNEL_ETH0TX);
// Issue a software request to start the channel running.
uDMAChannelRequest(UDMA_CHANNEL_ETH0TX);
// Wait for the previous transmission to be complete.
while((HWREGBITW(&g_ulFlags, FLAG_TXPKT) == 1) &&
EthernetSpaceAvail(ETH_BASE))
{
}
// Take back off the byte that we addeded above.
return(lBufLen - 1);
}
//*****************************************************************************
// Set up the pins that are used for Ethernet
//*****************************************************************************
void EthernetPinsSetup(void)
{
// MII_TXD3
GPIODirModeSet(GPIO_PORTC_BASE, GPIO_PIN_4, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTC_BASE, GPIO_PIN_4, GPIO_PIN_TYPE_STD);
HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL) &= 0xFFF0FFFF;
HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL) |= 0x00030000;
// MII_MDIO
GPIODirModeSet(GPIO_PORTE_BASE, GPIO_PIN_6, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTE_BASE, GPIO_PIN_6, GPIO_PIN_TYPE_STD);
HWREG(GPIO_PORTE_BASE + GPIO_O_APSEL)|= 0x00000040;
HWREG(GPIO_PORTE_BASE + GPIO_O_PCTL) &= 0xF0FFFFFF;
HWREG(GPIO_PORTE_BASE + GPIO_O_PCTL) |= 0x0C000000;
// MII_RXD3
GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_5, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_5, GPIO_PIN_TYPE_STD);
HWREG(GPIO_PORTF_BASE + GPIO_O_PCTL) &= 0xFF0FFFFF;
HWREG(GPIO_PORTF_BASE + GPIO_O_PCTL) |= 0x00300000;
// MII_TXER , MII_RXDV , MII_RXD1 , MII_RXD2
GPIODirModeSet(GPIO_PORTG_BASE, GPIO_PIN_7|GPIO_PIN_3|GPIO_PIN_1|GPIO_PIN_0,
GPIO_DIR_MODE_HW);
GPIOPadConfigSet(GPIO_PORTG_BASE, GPIO_PIN_7|GPIO_PIN_3|GPIO_PIN_1|
GPIO_PIN_0,
GPIO_PIN_TYPE_STD);
HWREG(GPIO_PORTG_BASE + GPIO_O_APSEL)|= 0x0000000B;
HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL) &= 0x0FFF0F00;
HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL) |= 0x3000C0CC;
// MII_TXCK , MII_TXEN , MII_TXD0 , MII_TXD1 , MII_TXD2 , MII_RXD0
GPIODirModeSet(
GPIO_PORTH_BASE, GPIO_PIN_7|GPIO_PIN_6|GPIO_PIN_5|GPIO_PIN_4|
GPIO_PIN_3|
GPIO_PIN_1, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(
GPIO_PORTH_BASE, GPIO_PIN_7|GPIO_PIN_6|GPIO_PIN_5|GPIO_PIN_4|
GPIO_PIN_3|
GPIO_PIN_1, GPIO_PIN_TYPE_STD);
HWREG(GPIO_PORTH_BASE + GPIO_O_APSEL)|= 0x000000C2;
HWREG(GPIO_PORTH_BASE + GPIO_O_PCTL) &= 0x00000F0F;
HWREG(GPIO_PORTH_BASE + GPIO_O_PCTL) |= 0xCC9990C0;
// MII_PHYRSTn , MII_PHYINTRn , MII_CRS , MII_COL , MII_MDC , MII_RXCK ,
// MII_RXER
GPIODirModeSet(
GPIO_PORTJ_BASE, GPIO_PIN_7|GPIO_PIN_6|GPIO_PIN_5|GPIO_PIN_4|
GPIO_PIN_3|
GPIO_PIN_2|GPIO_PIN_0, GPIO_DIR_MODE_HW);
GPIOPadConfigSet(
GPIO_PORTJ_BASE, GPIO_PIN_7|GPIO_PIN_6|GPIO_PIN_5|GPIO_PIN_4|
GPIO_PIN_3|
GPIO_PIN_2|GPIO_PIN_0, GPIO_PIN_TYPE_STD);
HWREG(GPIO_PORTJ_BASE + GPIO_O_APSEL)|= 0x000000FC;
HWREG(GPIO_PORTJ_BASE + GPIO_O_PCTL) &= 0x000000F0;
HWREG(GPIO_PORTJ_BASE + GPIO_O_PCTL) |= 0xCCCCCC03;
}
//*****************************************************************************
// respond to commands sent by the user (client)
//
//*****************************************************************************
void EthernetProcessCMD(int command)
{
static unsigned char toggle_LED6 = 0;
static unsigned char toggle_LED7 = 0;
switch(command)
{
case TOGGLE_LED_7:
toggle_LED7 = ~toggle_LED7;
GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_6, toggle_LED7);
break;
case TOGGLE_LED_6:
toggle_LED6 = ~toggle_LED6;
GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_7, toggle_LED6);
break;
case GET_LED6_STATUS:
if(GPIOPinRead(GPIO_PORTC_BASE,GPIO_PIN_7)& 0x80)
httpd_insert_response(sizeof(led6_off)-1,(char *)led6_off);
else
httpd_insert_response(sizeof(led6_on)-1,(char *)led6_on);
break;
case GET_LED7_STATUS:
if(GPIOPinRead(GPIO_PORTC_BASE,GPIO_PIN_6) & 0x40)
httpd_insert_response(sizeof(led7_off)-1,(char *)led7_off);
else
httpd_insert_response(sizeof(led7_on)-1,(char *)led7_on);
break;
default:
break;
}
}
//*****************************************************************************
// This example demonstrates the use of the Ethernet Controller with the uIP
// TCP/IP stack.
//*****************************************************************************
int
main(void)
{
uip_ipaddr_t ipaddr;
static struct uip_eth_addr sTempAddr;
long lPeriodicTimer, lARPTimer;
unsigned long ulUser0, ulUser1;
unsigned long ulTemp;
int command_word;
// Disable Protection
HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;
// Sets up PLL, M3 running at 100MHz and C28 running at 100MHz
SysCtlClockConfigSet(SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0xA) |
SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_1 |
SYSCTL_XCLKDIV_4);
// Remove This
// PinoutSet();
// Enable clock supply for the following peripherals
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
// Enable clock supply for the following peripherals
SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ETH);
// Disable clock supply for the watchdog modules
SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG1);
SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG0);
// Set up the 20 pins required for Ethernet communication
EthernetPinsSetup();
// Set up LED7 pin
GPIOPinTypeGPIOOutput(LED_0_BASE, LED_0_PIN);
GPIOPinWrite(LED_0_BASE, LED_0_PIN, 0);
// Set up LED6 pin
GPIOPinTypeGPIOOutput(LED_1_BASE, LED_1_PIN);
GPIOPinWrite(LED_1_BASE, LED_1_PIN, 0);
// Adjust the pointer to be aligned on an odd half word address so that
// DMA can be used.
uip_buf = (u8_t *)(((unsigned long)ucUIPBuffer + 3) & 0xfffffffe);
// Enable the uDMA controller and set up the control table base.
SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
uDMAEnable();
uDMAControlBaseSet(g_sDMAControlTable);
// Configure the DMA TX channel
uDMAChannelAttributeDisable(UDMA_CHANNEL_ETH0TX, UDMA_ATTR_ALL);
uDMAChannelControlSet(UDMA_CHANNEL_ETH0TX,
UDMA_SIZE_32 | UDMA_SRC_INC_32 |
UDMA_DST_INC_NONE | UDMA_ARB_8);
// Set user/company specific MAC octets
// (for this code we are using A8-63-F2-00-00-80)
// 0x00 MACOCT3 MACOCT2 MACOCT1
ulUser0 = 0x00F263A8;
// 0x00 MACOCT6 MACOCT5 MACOCT4
ulUser1 = 0x00800000;
// User needs to program user specific MAC address into Flash
// and read it on power up
if((ulUser0 == 0xffffffff) || (ulUser1 == 0xffffffff))
{
// We should never get here. This is an error if the MAC address has
// not been programmed into the device. Exit the program.
while(1)
{
}
}
// Enable and Reset the Ethernet Controller.
SysCtlPeripheralEnable(SYSCTL_PERIPH_ETH);
SysCtlPeripheralReset(SYSCTL_PERIPH_ETH);
// Configure SysTick for a periodic interrupt.
SysTickPeriodSet(SysCtlClockGet(SYSTEM_CLOCK_SPEED) / SYSTICKHZ);
SysTickEnable();
IntRegister(FAULT_SYSTICK, SysTickIntHandler);
SysTickIntEnable();
// Configure the DMA channel for Ethernet receive.
uDMAChannelAttributeDisable(UDMA_CHANNEL_ETH0RX, UDMA_ATTR_ALL);
uDMAChannelControlSet(UDMA_CHANNEL_ETH0RX,
UDMA_SIZE_32 | UDMA_SRC_INC_NONE |
UDMA_DST_INC_32 | UDMA_ARB_8);
// Initialize the Ethernet Controller and disable all Ethernet Controller
// interrupt sources.
EthernetIntDisable(ETH_BASE, (ETH_INT_PHY | ETH_INT_MDIO |
ETH_INT_RXER | ETH_INT_RXOF |
ETH_INT_TX | ETH_INT_TXER | ETH_INT_RX));
ulTemp = EthernetIntStatus(ETH_BASE, false);
EthernetIntClear(ETH_BASE, ulTemp);
// Initialize the Ethernet Controller for operation.
EthernetInitExpClk(ETH_BASE, SysCtlClockGet(SYSTEM_CLOCK_SPEED));
// Configure the Ethernet Controller for normal operation.
// - Full Duplex
// - TX CRC Auto Generation
// - TX Padding Enabled
EthernetConfigSet(ETH_BASE, (ETH_CFG_TX_DPLXEN | ETH_CFG_TX_CRCEN |
ETH_CFG_TX_PADEN));
// Wait for the link to become active.
while((EthernetPHYRead(ETH_BASE, PHY_MR1) & 0x0004) == 0)
{
}
// Enable the Ethernet Controller.
EthernetEnable(ETH_BASE);
// Enable and register the Ethernet interrupt.
IntRegister(INT_ETH, EthernetIntHandler);
IntEnable(INT_ETH);
// Enable the Ethernet RX Packet interrupt source.
EthernetIntEnable(ETH_BASE, ETH_INT_RX);
// Enable all processor interrupts.
IntMasterEnable();
// Initialize the uIP TCP/IP stack.
uip_init();
#ifdef USE_STATIC_IP
uip_ipaddr(ipaddr, DEFAULT_IPADDR0, DEFAULT_IPADDR1, DEFAULT_IPADDR2,
DEFAULT_IPADDR3);
uip_sethostaddr(ipaddr);
ShowIPAddress(ipaddr);
uip_ipaddr(ipaddr, DEFAULT_NETMASK0, DEFAULT_NETMASK1, DEFAULT_NETMASK2,
DEFAULT_NETMASK3);
uip_setnetmask(ipaddr);
#else
uip_ipaddr(ipaddr, 0, 0, 0, 0);
uip_sethostaddr(ipaddr);
uip_ipaddr(ipaddr, 0, 0, 0, 0);
uip_setnetmask(ipaddr);
#endif
// Convert the 24/24 split MAC address from ram into a 32/16 split MAC
// address needed to program the hardware registers, then program the MAC
// address into the Ethernet Controller registers.
sTempAddr.addr[0] = ((ulUser0 >> 0) & 0xff);
sTempAddr.addr[1] = ((ulUser0 >> 8) & 0xff);
sTempAddr.addr[2] = ((ulUser0 >> 16) & 0xff);
sTempAddr.addr[3] = ((ulUser1 >> 0) & 0xff);
sTempAddr.addr[4] = ((ulUser1 >> 8) & 0xff);
sTempAddr.addr[5] = ((ulUser1 >> 16) & 0xff);
// Program the hardware with it's MAC address (for filtering).
EthernetMACAddrSet(ETH_BASE, (unsigned char *)&sTempAddr);
uip_setethaddr(sTempAddr);
// Initialize the TCP/IP Application (e.g. web server).
httpd_init();
#ifndef USE_STATIC_IP
// Initialize the DHCP Client Application.
dhcpc_init(&sTempAddr.addr[0], 6);
dhcpc_request();
#endif
// Main Application Loop.
lPeriodicTimer = 0;
lARPTimer = 0;
httpd_clear_command();
while(true)
{
// Wait for an event to occur. This can be either a System Tick event,
// or an RX Packet event.
while(!g_ulFlags)
{
}
// If SysTick, Clear the SysTick interrupt flag and increment the
// timers.
if(HWREGBITW(&g_ulFlags, FLAG_SYSTICK) == 1)
{
HWREGBITW(&g_ulFlags, FLAG_SYSTICK) = 0;
lPeriodicTimer += SYSTICKMS;
lARPTimer += SYSTICKMS;
}
// Check for an RX Packet and read it.
if(HWREGBITW(&g_ulFlags, FLAG_RXPKT))
{
// Get the packet and set uip_len for uIP stack usage.
uip_len = (unsigned short)EthernetPacketGetDMA(ETH_BASE, uip_buf,
sizeof(ucUIPBuffer));
// Clear the RX Packet event and re-enable RX Packet interrupts.
if(HWREGBITW(&g_ulFlags, FLAG_RXPKT) == 1)
{
HWREGBITW(&g_ulFlags, FLAG_RXPKT) = 0;
EthernetIntEnable(ETH_BASE, ETH_INT_RX);
}
// Process incoming IP packets here.
if(BUF->type == htons(UIP_ETHTYPE_IP))
{
uip_arp_ipin();
uip_input(); //uip_process (calls uip_appcall())
if(httpd_get_command(&command_word))
{
httpd_clear_command();
EthernetProcessCMD(command_word);
}
// If the above function invocation resulted in data that
// should be sent out on the network, the global variable
// uip_len is set to a value > 0.
if(uip_len > 0)
{
uip_arp_out();
EthernetPacketPutDMA(ETH_BASE, uip_buf, uip_len);
uip_len = 0;
}
}
// Process incoming ARP packets here.
else if(BUF->type == htons(UIP_ETHTYPE_ARP))
{
uip_arp_arpin();
// If the above function invocation resulted in data that
// should be sent out on the network, the global variable
// uip_len is set to a value > 0.
if(uip_len > 0)
{
EthernetPacketPutDMA(ETH_BASE, uip_buf, uip_len);
uip_len = 0;
}
}
}
// Process TCP/IP Periodic Timer here.
if(lPeriodicTimer > UIP_PERIODIC_TIMER_MS)
{
lPeriodicTimer = 0;
for(ulTemp = 0; ulTemp < UIP_CONNS; ulTemp++)
{
uip_periodic(ulTemp);
// If the above function invocation resulted in data that
// should be sent out on the network, the global variable
// uip_len is set to a value > 0.
if(uip_len > 0)
{
uip_arp_out();
EthernetPacketPutDMA(ETH_BASE, uip_buf, uip_len);
uip_len = 0;
}
}
#if UIP_UDP
for(ulTemp = 0; ulTemp < UIP_UDP_CONNS; ulTemp++)
{
uip_udp_periodic(ulTemp);
// If the above function invocation resulted in data that
// should be sent out on the network, the global variable
// uip_len is set to a value > 0.
if(uip_len > 0)
{
uip_arp_out();
EthernetPacketPutDMA(ETH_BASE, uip_buf, uip_len);
uip_len = 0;
}
}
#endif
}
// Process ARP Timer here.
if(lARPTimer > UIP_ARP_TIMER_MS)
{
lARPTimer = 0;
uip_arp_timer();
}
}
}