Other Parts Discussed in Thread: TMS320F28062F, TMS320F28062
Hi,
I'm trying 80-pin TMS320F280F28062F, but not make sure some pins' usage. The following is my question.
(1) Just like to make sure one thing.... TMS320F280F28062 and TMS320F280F28062F has almost the same function. The only difference between them is that TMS320F280F28062F provides FOC algorithm embedded into its ROM for usage. Is it true?
(2) Can I operate this MCU without X1(pin-48) and X2(pin-47)? If yes, should I have X1 tied to Ground and X2 float?
(3) If I do not use the internal VREG for MCU, do I have to keep all VDDIO pins unconnected? and have VREGNZ pull high?
Thanks!