Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I have solar explorer kir TMDSCSOLAREXPKIT Concerto type, I load the gui via ethernet cable, I saw the bulb is lighting, everything was good. But When I try to measure the PWM, something happen and bulb light gone. I restart the GUI do everything same but inver stage did not work. Then I load the PV Inverter program I load the program and debug the code apply the same stages in the control suite pdf. However, when change the LightCommand and the Inv_Iset the thoretical panel power cahnge also panel voltage change but the other variables are seems zero. I can't get any PWM signals.. Please help.. Is there any training video or extra detailed information about working on DC-DC boost PWM stage.
Thank you..
Zekiye