Hi,
One question, please . Can the C2000 solar inverter development kit output the AC current sine wave THD<3% with the reference software ?
Thanks,
Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Leo,
According to the doc available for the above kit in control suite it says:
1.1 Specification
The system main spec is below:
Power Rating: 600W.
Norminal Grid Voltage: 120V/60Hz(RMS), 220V/50Hz.
Output Power Factor: 1.
THDi: <5%.
Panel Input Voltage Range: 400V.
Grid Tie.
Anti-islanding Protection.
Test Condition:
AC source connected, with 120VAC/60Hz;
DC bus voltage: 400V
Power range: 100-600W output;
Grid-Tie.
Room Temperature
Regards,
Gautam
Hi Gautam
I have checked that your answer is from the document <High Voltage Solar Inverter DC-AC Kit>, the development kit is TMDSHV1PHINVKIT .
what about the TMDSSOLARCEXPKIT and TMDSSOLARPEXPKIT ? I have not found the test result of this development kit . I want to make sure THDi of these kit.
Thanks,
Leo
Leo,
Unfortunately no such measurement was done for the solar explorer kit, as the focus was explaining the concept and quick learning of the controller,
the power stages and control loops are better tuned for the HV kit and the data of which was pointed out in the previous post,
Regards
Manish Bhardwaj