Hi,
I bought TI's EVM (TMDSHV1PHINVKIT) and debugged TI's code(SolarHv_DCAC_PiccoloB_Rev_02) in the control card
then tested according to the quick start guide but it did not work in build=3.
My output result is shown below (blue: ac source voltage , purple: inverter output current)
it's easy to see that the output current is not locked on ac voltage.
Does output current start at the zero crossing point?
If yes, where can I find the corresponding portions of the codes ?
Thanks a lot