This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MPEG-L3 decoder in F28069!!!

Hi,

  I'm implementing MP3 decoder in F28069. I referring source code from http://embdev.net/articles/ARM_MP3/AAC_Player . I found some WindowsOS related Data types.

in the following files.

* MULSHIFT32(x, y) signed multiply of two 32-bit integers (x and y),
* returns top 32-bits of 64-bit result
* CLIPTOSHORT(x) convert 32-bit integer to 16-bit short,
* clipping to [-32768, 32767]
* FASTABS(x) branchless absolute value of signed integer x
* CLZ(x) count leading zeros on signed integer x
* MADD64(sum64, x, y) 64-bit multiply accumulate: sum64 += (x*y)