Other Parts Discussed in Thread: TMS320F28035, UNIFLASH
Hi,
I have a tested a TMS320F28035 project getting ready to go to production. So far I was using Debug to flash my program.
I was trying to flash my target program using CCS Uniflash 2.2.0. for the first time.
It failed but now I cant use "Debug" on my Code Composer Studio Version: 5.2.1.00018 anymore.
I get the following error message:
C28xx: Error connecting to the target: (Error -233 @ 0x0) The JTAG IR and DR scan-paths cannot circulate bits, they may be broken. An attempt to scan the JTAG scan-path has failed. The target's JTAG scan-path appears to be broken with a stuck-at-ones or stuck-at-zero fault. (Emulation package 5.0.471.0)
Tried Resseting everything 20 times including the computer without success. I am using a Blackhawk USB2000 emulator.
I hope I didn't brick my Piccolo. Can anybody help ???
Thanks,
Danny