Other Parts Discussed in Thread: CONTROLSUITE
I am having some issues getting signals out of some PWMs on the F28M36.
Our custom hardware is designed with PWM7a assigned to GPIO124, PWM7b to GPIO125, etc up to GPIO129 in order to drive a three phase inverter.
We have given the C2000 core control of the R and S GPIO ports from the M3 side and we have enabled the bits in the C2000 GPIOMUXD and GPIOMUXE registers.
We have tried enabling them according to table 4-47 in the TRM and we have also tied enabling them with a bit setting of 01b.
We are turning off protection during the IO setup with the EALLOW command however it seems no matter what we try we don’t get any signal.
One thing that scares me is table 4-58 in the TRM does not list PWMs as functions on GPIO24-GPIO29 even though table 4-47 does and they are listed as functions in the F28M36 datasheet (which we originally used to create our MAP).
Has anyone had any luck enabling PWMs on GPIO124-GPIO129?
Thanks!