Other Parts Discussed in Thread: TMS320F28035
Someone can help me to understand this example on a TMS320F28035 ?
Ok, when I launch it no problem everyting works.
But I don't really understand WHERE the data is written...
Indeed, in the I2cMsgOut1 struct I have two adresses : I2C_EEPROM_HIGH_ADDR and I2C_EEPROM_LOW_ADDR (0x00 & 0x30) then I have two data to write (0x12 & 0x34)
then in the "I2CA_WriteData" function I can see this code who write the data on the I2C bus :
I2caRegs.I2CDXR = msg->MemoryHighAddr;
I2caRegs.I2CDXR = msg->MemoryLowAddr;
// for (i=0; i<msg->NumOfBytes-2; i++)
for (i=0; i<msg->NumOfBytes; i++)
{
I2caRegs.I2CDXR = *(msg->MsgBuffer+i);
}
So if I understand the datas send on the I2C bus are => I2C_ADDR 0x00 0x30 0x12 0x34 ? I'm right ?
So where are stored my datas ? is Adresse 0x00 ==0x12 and 0x30 ==0x34 ? OR adresse 0x30 ==0x12 and 0x31 == 0x34 ??
Thank you.
Best regards, Nicolas