Hi everyone,
Even after the reading of http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/146974.aspx and http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/21202.aspx I still have some issues with my FixedPoint FFT (my previous floating point was working well).
Here is my code :
#include "fft.h"
#define FFT_SIZE 1024
// FFT SECTIONS
RFFT32 fft=RFFT32_1024P_DEFAULTS;
#pragma DATA_SECTION(Fft_in,"FFTIN");
long Fft_in[2*FFT_SIZE];
#pragma DATA_SECTION(Spectro,"FFTOUT");
long Spectro[(FFT_SIZE/2)+1];
// FFT CALCULATION
void realfft(void)
{
fft.ipcbptr=Fft_in;
fft.magptr=Spectro;
fft.init(&fft);
RFFT32_brev(Fft_in,Fft_in,FFT_SIZE);
fft.calc(&fft);
fft.mag(&fft);
}
And my magnitude buffer Spectro stays empty... Should I move on CFFT32 like Vishal said in the other topic ? Or do you find any error that could explain that ?
Btw, I didn't really understand how this RFFT works (when the Floating Point FFT is logical, this one is hard to understand), if you have further explanation, I'd be glad to read them ! (datasheet read and re-read).
Regards,
Alex