I plugged in the launchpad and when I executed the ADCSOC example program the launchpad stopped working. The LEDs slowly dimmed away so I touched the board to hit the reset button and felt that it was heated up. The following error message showed up on the CCS console:
C28xx: Error: (Error -154 @ 0x0) One of the FTDI driver functions used to write data returned bad status or an error. (Emulation package 5.1.73.0).
Another error message also showed up saying that a board was not recognized or plugged in after the LEDs dimmed away.
I made sure the voltage being passed in was under 1V and so it wasn't overloaded and the grounds were correctly in place. Is there an explanation as to why this happened? I have also tried loading the other demos or examples and the same thing happens.