This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35x- EPI interface

Hi,

In the EPI interface, how to put the Address and Data in muxed communication. While putting the Address i need to pull the ALE line low. If i put the address and data in 0xA0000000, only my data is going. And my CS also not changed.

Please help me to fix this

Thirumoorthy.R

  • Hi Thirumoorthy,

    Can you please check your code and confirm if the setting of MODE filed of EPIHB8CFG/EPIHB16CFG register is correct to use the address/data mux option.

     

    Regards,

    Vivek Singh

  • Hi vivek,

    Yes, I checked. My Configuration is like this ,

    EPIHB8CFG = 0x00000000;

    EPIHB8CFG2 = 0x03000000;

    And my EPIADDR is 0x00000055;

    I checked my ALE line and WR line. It is correct only.

    My slave device will accept the address only when the ALE and WR line is LOW. But when i am sending the Address my ALE is in LOW state but WR line wont go to LOW

    state.

    My slave device write sequence  is like this:

    .

    But my EPI write like this,

    Please help me to configure my F28M3H52C1 , like both ALE and WR should LOW while writing the Address. And WR should LOW while writing the Data. My chip select (CS1) looking correctly. My CS1 is low when i am writing the Address & Data.

    I have a problem in EPI with my slave device. My slave device is S1D13742 using Host bus 8 bit interface. 

    I am using HB8 mode with ALE & 2 CSn pin. Is it possible to change the state of WR while writing the Address. My slave device accept the Address only when the ALE and WR in LOW. 

    Thirumoorthy.R