This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 I2c Write Function

Does anyone have an I2C write function that they would care to share?

  • Hi Kenton,

    Assuming you have a F28335 mcu and you are interfacing it with an EEPROM; here's how i2c write is implemented :

    Uint16 I2CA_WriteData(struct I2CMSG *msg)
    {
    Uint16 i;

    // Wait until the STP bit is cleared from any previous master communication.
    // Clearing of this bit by the module is delayed until after the SCD bit is
    // set. If this bit is not checked prior to initiating a new message, the
    // I2C could get confused.
    if (I2caRegs.I2CMDR.bit.STP == 1)
    {
    return I2C_STP_NOT_READY_ERROR;
    }

    // Setup slave address
    I2caRegs.I2CSAR = msg->SlaveAddress;

    // Check if bus busy
    if (I2caRegs.I2CSTR.bit.BB == 1)
    {
    return I2C_BUS_BUSY_ERROR;
    }

    // Setup number of bytes to send
    // MsgBuffer + Address
    I2caRegs.I2CCNT = msg->NumOfBytes+2;

    // Setup data to send
    I2caRegs.I2CDXR = msg->MemoryHighAddr;
    I2caRegs.I2CDXR = msg->MemoryLowAddr;
    // for (i=0; i<msg->NumOfBytes-2; i++)
    for (i=0; i<msg->NumOfBytes; i++)

    {
    I2caRegs.I2CDXR = *(msg->MsgBuffer+i);
    }

    // Send start as master transmitter
    I2caRegs.I2CMDR.all = 0x6E20;

    return I2C_SUCCESS;
    }

    Regards,

    Gautam

  • I have a C2803 and I am interfacing with an encoder device (Slave address @ 0x40).  

    This routine looks similar to the I2C_eeprom example.  I was not able to get your code or the I2c_eeprom to work with my device.