Other Parts Discussed in Thread: TMS320F28335, TL16C754B
Hi,
I am designing a delfino TMS320f28335 based board where I need 4 external uarts (excluding 3-internal uarts of delfino microcontroller)
I was planning to use T.I's TL16C754B Quad Uart (having 8-Bit Asynchronous Interface) for it.
However the XINTF interface of TMS320f28335 delfino microcontroller only supports 16-Bit and 32-Bit asynchronous interfaces.
I wanted to ask that can I still use XINTF (some how) to interface the 8-bit asynchronous mode for said Quad Uart ?
I have attached an example connectivity diagram, so any body could guide me whether it is possible or not.