Hello Lori:
I have a concerto control card. I would to connect to the SCI port of the dsp. I can't find where th TX and RX of the SCI come out that I can connect to them and communicate with the SCI.
Regards Arye
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Lori:
I have a concerto control card. I would to connect to the SCI port of the dsp. I can't find where th TX and RX of the SCI come out that I can connect to them and communicate with the SCI.
Regards Arye
The collateral, including documentation for both software and hardware for the control card, can be obtained through installation of controlSUITE.
The product folder of the control card has some information regarding this.
Hello Igor :
In that document you can't find the SCI TX. I want to communicate with the SCI with a PC. The RX signal is available but the TX I can't find.
Regards Arye
Hello Brandon:
I looked in the controlSuite but I can't find the TX signal that I can connect to it.
Regards Arye
Sorry Arje, but it is all in the controlsuite - pdf (C:\ti\controlSUITE\development_kits\~controlCARDs\CCF28M35xxHWdevPkg_v2\R_PWB_RevD)
SCI-RX : mini-USB -> FTDI-Chip (U15- Pin38) - > ISO (U21_PIN2) -> U21-Pin7 -> SW3-Pin2 -> SW3 - Pin3 -> PE4_GPIO28
SCI-TX: PE4_GPIO29 -> ISO (U22 - PIN2) -> U22-Pin7 -> FTDI-Chip (U15-Pin 39) -> mini-USB