This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 Rev0 vs RevB inconsistent behavior

We have boards with Rev0 F28M35 devices and recently received  boards with RevB F28M35 devices.

We are running the same code on Rev0 boards as RevB. After initial device setup we use a UART to initialize an external device then talk on Ethernet. On the Rev0 boards it takes 1.5sec to the point at which we talk on Ethernet, on the RevB boards this takes 150sec. A factor of 100.

Has anyone seen this type of behavior?