Hello, I would like to make eCAP module synchronized with ePWM module in 28069.
However, I cannot find how to make it with the information in the Technical Reference Manual.
From 3.2.2.3.3, Time-Base Counter Synchronization part, 28069 is constructed with the structure in Fig. 3-7, Time-Base Counter Synchronization Scheme 1.
In FIg. 3-7. eCAP1 module can be synchronized with ePWM1 by using EPWM1SYNCO signal.
Q1. Here, could you tell me how I can enable this synchronization? Just enabling EPWM1SYNCO and SYNCI in eCAP1 module make it possible?
Any connections in hardware is required?
Q2. How can I make eCAP1, ..., eCAPn modules synchronized?
From Fig. 6-6, Details of the Counter and Synchronization Block, it can be noted that SYNCI signal can be passed through and used as SYNCO signal.
In 28069, sync signals of eCAP1, ..., eCAPn modules are chained like ePWM modules?
Thank you very much in advance.