Other Parts Discussed in Thread: TMS320F28335, TMS320F2802, MOTORWARE
Using a TMS320F28335 with the following settings
SYSCLKOUT = 144MHz
IPSC = 11
ICCL = 10
ICCH = 10
Using the formulae given in sprug03b sections 1.4 and 5.7.1, I expect
Module Clock = 12 MHz and Master Clock = 400kHz.
Using a ‘scope we see SYSCLOCKOUT is 144MHz as set, but the clock out on the I2C bus is approx 360kHz.
Any idea as to what might be happening here?
Looking at the data and clock signals we are seeing unexpected “stop” transitions. Could this be due to the the expected 400kHz clock vs. the actual 360kHz clock?
Regards.