Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hello,
I really need help , i am still a learner and this is the task given.
I am working with Instaspin FOC drv8301 kit
my motor which has rated voltage 18V .
when working with automatic ID I change the identification parameters accordingly , my motor spins and gets identified. Some times it stops at EST_STATE_Ramp down
Is the identified parameters correct ?
If so ,now my next step is that i should update this in user.h and compile
I am unable to do that.
Can anyone help how to do this or suggest any references ?
If anyone helps me out i will be really glad and grateful
Thankyou in advance
Archana Lokesh