This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Chassis For TMDSHVMPPTKIT and TMDSHV1PHINVKIT

Hello TI,

I just received the above - I thought they came with the chassis shown in the following pics:

Does anyone know what the P/N's are for the above chassis'?

Thanks In Advance,
johnw 

  • John,

    This was our intention as well.  However, because of legal concerns based around regulatory compliance (we do not want to be classified as an end product) it was recommended that we not include the enclosure.

    We do not supply chassis/enclosures for these EVMs.  Do you have a specific concern?


    Thank you,
    Brett

  • Hello Brett,

    Well, since they are depicted that way - one is led to believe the EVM's include the chassis in the pictures.

    Yes - my concern at the moment is that I do not know the P/N's for those chassis' and it would be a lot easier if TI could give them to me vs. 'hunting' for them
    via the Internet.

    So, can you please give me the P/N's?

    Thanks!
    johnw 

  • John,

    We worked with a third-party to have these enclosures custom-made for these specific kits.  We/they never expected to sell these independently so there isn't a part number.

    The best I could do is get you the name of the manufacturer who we worked with and they should be able to pull up all the CAD information.  However, because these never went into production I can't guarantee getting one will be very cheap.  Let me know...

    I'll submit a bug to change out pictures in our documentation.


    Thank you,
    Brett