I've got two units that do constant resets (see waveform). The reset line drops down for a period of about 5 microseconds and does this at a rate of 757 Hz in both units. Everything was removed from the reset line except the pull up to 3.3V and the units still do this. We can't program either unit. The microprocessor was replaced in both cases and we get the same result. What could cause this? I'm sure it's something on our board as none of our other units do this. However, we're not drawing excessive current, the 3.3V and 1.8V are steady and in tolerance, and the oscillator is steady at 100MHz. The processor is seeing something it doesn't like and I don't know where to start looking.
I'm stumped.