This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reading data from EEPROM using I2C without interrupts



Hello,

I am writing code to read and write data from an EEPROM using I2C without the use of interrupts. Due to project constraints, I cannot use interrupts.

I have confirmed my read function works correctly. I am able to write to my eeprom using different code and read it back using my read function.

However, my write function does not work correctly. For example, when I write 0x3A to a memory location I read back 0xCC. Since I have confirmed the read function works ok, I believe my write function is the source of the incorrect read data.

Any help would be appreciated.

Below is the is the write function:

 

// Read data from EEPROM using polling instead of interrupts

void I2cRx(structI2CMSG *msg)

{

Uint16 i;

// Wait until the STP bit is cleared from any previous master communication.

// Clearing of this bit by the module is delayed until after the SCD bit is

// set. If this bit is not checked prior to initiating a new message, the

// I2C could get confused.

if (I2caRegs.I2CMDR.bit.STP == 1)

{

I2caRegs.I2CMDR.bit.STP = 0;

}

I2caRegs.I2CSAR = 0x0050;

// Check if bus busy

while(I2caRegs.I2CSTR.bit.BB == 1){}

I2caRegs.I2CCNT = 2;

I2caRegs.I2CDXR = msg->MemoryHighAddr;

I2caRegs.I2CDXR = msg->MemoryLowAddr;

I2caRegs.I2CMDR.all = 0x2620; // orig 0x2620. Send data to setup EEPROM address

while(I2caRegs.I2CSTR.bit.ARDY == 0)

{

// wait until communication complete and registers ready

}

I2caRegs.I2CCNT = msg->NumOfBytes; // Setup how many bytes to expect

I2caRegs.I2CMDR.all = 0x2C20; // originally 0x2C20. Send restart as master receiver

while(I2caRegs.I2CFFRX.bit.RXFFINT == 0)

{

// wait until I2CDRR is ready to be read

}

//Clear message buffer for debugging purposes to ensure correct data is read from I2CDRR.

for(i=0; i < I2C_NUMBYTES; i++)

{

CurrentMsgPtr->MsgBuffer[i] = 0;

}

for(i=0; i < I2C_NUMBYTES; i++)

{

CurrentMsgPtr->MsgBuffer[i] = I2caRegs.I2CDRR;

}

}