Hello.
I am using a TMS320F028016PZA with CCSv3.3. I am trying to implement eCAN, working for the example files (A_to_B_Xmit and back_to_back), but right now I can't transmit any frame.
In order to know where the problem is, I saw the signal TX with an oscilloscope (pin 7), and the level didn't change. But I couldn't believe when I saw the signal had 1V level. I hoped 0V (low level) and 3,3V (high level).
After that, I have checked the voltage in other pins and I get 3,3V as I would have expected. Any idea?